Skip to main content
Senior
September 15, 2024
Question

[SOLVED] - CubeIDE not downloading and restoring previously downloaded code

  • September 15, 2024
  • 0 replies
  • 1094 views

[SOLVED - It was a bouncy ground on the programming connector on the second PCB]

 

Hi,

I have two version of the same PCB only with minor HW differences which also require minor SW differences. So I made a copy of a project folder that works and renamed the folder. Then in CubeMX I also renamed the project itself.

 

It compiles but when I try to download it onto the micro - using the same Segger's J-Link I always use - it:

1) does not download the code onto the micro

2) instead of opening the source code window it shows error:

No source available for "(gdb[6].proc[42000].threadGroup[i1],gdb[6].proc[42000].OSthread[1]).thread[1].frame[0]"

but the main() source file (and other ones) are there and already opened.

3) it restarts the PCB running the old code (extremely different in functionality including which LEDs are on, so it's very obvious it is the old code)

 

The output window is shown below. From the output window, it seems the communication between the J-Link and the PCB is ok, which also seems to be confirmed by the fact that CubeMXProgrammer does read the chip memory.

 

But even in that output window it shows some errors. What might be the cause?

 

This is the full output:

 

 

 

 

SEGGER J-Link GDB Server V7.84e Command Line Version

JLinkARM.dll V7.84e (DLL compiled Feb 1 2023 16:41:41)

Command line: -port 2331 -s -device STM32L452RE -endian little -speed 4000 -if swd -vd
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: off
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: STM32L452RE
Target device parameters: none
Target interface: SWD
Target interface speed: 4000kHz
Target endian: little

Connecting to J-Link...
J-Link is connected.
Firmware: J-Link V11 compiled May 28 2024 15:36:02
Hardware: V11.00
S/N: 261014476
OEM: SEGGER-EDU
Feature(s): FlashBP, GDB
Checking target voltage...
Target voltage: 3.24 V
Listening on TCP/IP port 2331
Connecting to target...
Halting core...
Connected to target
Waiting for GDB connection...Connected to 0000:0000:0000:0000:0000:0000:0000:0001
GDB client (conn. 1120) requested target.xml from GDB Server
Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x4E510000
Read register 'r1' (4 bytes) from hardware: 0x00100000
Read register 'r2' (4 bytes) from hardware: 0xD1070000
Read register 'r3' (4 bytes) from hardware: 0x5B030000
Read register 'r4' (4 bytes) from hardware: 0x10010020
Read register 'r5' (4 bytes) from hardware: 0x00000000
Read register 'r6' (4 bytes) from hardware: 0x00000000
Read register 'r7' (4 bytes) from hardware: 0xE07F0220
Read register 'r8' (4 bytes) from hardware: 0x00000000
Read register 'r9' (4 bytes) from hardware: 0x00000000
Read register 'r10' (4 bytes) from hardware: 0x00000000
Read register 'r11' (4 bytes) from hardware: 0x00000000
Read register 'r12' (4 bytes) from hardware: 0x00000000
Read register 'sp' (4 bytes) from hardware: 0xDC7F0220
Read register 'lr' (4 bytes) from hardware: 0x690D0008
Read register 'pc' (4 bytes) from hardware: 0x260D0008
Read register 'xpsr' (4 bytes) from hardware: 0x00000021
Read 4 bytes @ address 0x08000D26 (Data = 0x4B03AF00)
Reading 64 bytes @ address 0x20027FC0
Received monitor command: ReadAPEx 0x0 0xF8
O.K.:0xE00FF003
Received monitor command: ReadMemAP 0x0 0xE00FFFD0 0x8 0x0
O.K.:0x00000000,0x00000000,0x00000000,0x00000000,0x00000062,0x00000004,0x0000000A,0x00000000
Connected to 0000:0000:0000:0000:0000:0000:0000:0001
GDB client (conn. 1140) requested target.xml from GDB Server
Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x4E510000
Read register 'r1' (4 bytes) from hardware: 0x00100000
Read register 'r2' (4 bytes) from hardware: 0xD1070000
Read register 'r3' (4 bytes) from hardware: 0x5B030000
Read register 'r4' (4 bytes) from hardware: 0x10010020
Read register 'r5' (4 bytes) from hardware: 0x00000000
Read register 'r6' (4 bytes) from hardware: 0x00000000
Read register 'r7' (4 bytes) from hardware: 0xE07F0220
Read register 'r8' (4 bytes) from hardware: 0x00000000
Read register 'r9' (4 bytes) from hardware: 0x00000000
Read register 'r10' (4 bytes) from hardware: 0x00000000
Read register 'r11' (4 bytes) from hardware: 0x00000000
Read register 'r12' (4 bytes) from hardware: 0x00000000
Read register 'sp' (4 bytes) from hardware: 0xDC7F0220
Read 4 bytes @ address 0x00000000 (Data = 0x20028000)
Read register 'lr' (4 bytes) from hardware: 0x690D0008
Read register 'pc' (4 bytes) from hardware: 0x260D0008
Read register 'xpsr' (4 bytes) from hardware: 0x00000021
Read 4 bytes @ address 0x08000D26 (Data = 0x4B03AF00)
Reading 64 bytes @ address 0x20027FC0
Received monitor command: reset
Resetting target
Downloading 404 bytes @ address 0x08000000 - Verified OK
Downloading 16048 bytes @ address 0x080001A0 - Verified OK
Downloading 15984 bytes @ address 0x08004050 - Verified OK
Downloading 14736 bytes @ address 0x08007EC0 - Verified OK
Downloading 1300 bytes @ address 0x0800B850 - Verified OK
Downloading 8 bytes @ address 0x0800BD64 - Verified OK
Downloading 4 bytes @ address 0x0800BD6C - Verified OK
Downloading 4 bytes @ address 0x0800BD70 - Verified OK
Downloading 1180 bytes @ address 0x0800BD74 - Verified OK
Writing register 'pc' = 0x08002B9C
ERROR: Failed to download RAMCode.
Failed to prepare for programming.
Failed to download RAMCode!
Read 4 bytes @ address 0x08002B9C (Data = 0xBF00621A)
Read 2 bytes @ address 0x08002B9C (Data = 0x621A)
Starting target CPU...
GDB closed TCP/IP connection (Socket 1140)
Debugger requested to halt target...
...Target halted (PC = 0x08000D70)
Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x16000000
Read register 'r1' (4 bytes) from hardware: 0x01000000
Read register 'r2' (4 bytes) from hardware: 0xC9000000
Read register 'r3' (4 bytes) from hardware: 0x15000000
Read register 'r4' (4 bytes) from hardware: 0x10010020
Read register 'r5' (4 bytes) from hardware: 0x00000000
Read register 'r6' (4 bytes) from hardware: 0x00000000
Read register 'r7' (4 bytes) from hardware: 0xE07F0220
Read register 'r8' (4 bytes) from hardware: 0x00000000
Read register 'r9' (4 bytes) from hardware: 0x00000000
Read register 'r10' (4 bytes) from hardware: 0x00000000
Read register 'r11' (4 bytes) from hardware: 0x00000000
Read register 'r12' (4 bytes) from hardware: 0x00000000
Read register 'sp' (4 bytes) from hardware: 0xE07F0220
Read register 'lr' (4 bytes) from hardware: 0x690D0008
Read register 'pc' (4 bytes) from hardware: 0x700D0008
Read register 'xpsr' (4 bytes) from hardware: 0x00000021
Read 4 bytes @ address 0x08000D70 (Data = 0xEC7F429A)
Reading 64 bytes @ address 0x20027FC0
GDB closed TCP/IP connection (Socket 1120)
Restoring target state and closing J-Link connection...
Shutting down...

 

 

 

 

Thank you

 

 

This topic has been closed for replies.