Skip to main content
JChou.1
Associate III
July 21, 2020
Question

SMBUS driver not working STM32F446

Hi there...

I'm trying to read(in blocking communication) battery related parameters on 2 wire SMBUS on a battery through Nucleo-F446ze and also on a custom board with stm32f446vc, but only interrupt "HAL_SMBUS_MasterTxCpltCallback" triggering, but no "HAL_SMBUS_MasterRxCpltCallback". With callback "HAL_SMBUS_ErrorCallback" I can see the smbus state changing to "HAL_SMBUS_STATE_RESET" and bus error "HAL_SMBUS_ERROR_TIMEOUT" , however as i communicating on smbus in blocking way, both the error should not be appearing.

With a discovery board "stm32f3-discovery", I able to read the battery parameters without any issue!!!

I'm configured my project in STMCubeIDE and STM32Cube_FW_F4_V1.25.0, I will appreciate for any help regarding same.

Thanks

This topic has been closed for replies.