Skip buildsteps during headless build
Hi,
i create a pipeline to compile a cubeide project with the cubeide in a docker container. on azure.
the docker container is linux based as i found no solution to do a headless cubeide installation on windows(or is there a way?)
in my project settings one of the build steps is to call a batch file for some code generation stuff. (this is needed during development so it does not get forgotten) normal development happens on a windows system.
(it would not be necessary to do the codegeneration step if the project is compiled on the buildserver)
as expected this does not work if i start the batch file in the linux headless build environment and it throws a error code
is there a way to skip this buildstep somehow? because at the moment this steps generates an error exit code which fails my complete build pipeline.
to discard every errorcode is not an option because i cannot distinguish between a compile error and a buildstep error (or am i missing sth?)
regards