Skip to main content
Abin
Associate III
August 2, 2023
Question

Showing clock incompatibility while selecting USB_OTG_FS in STM32F205VE

Hai ,

I enabled USB_OTG_HS in STM32F205VE and default frequency as 15 MHz. At this situation , It is showing the Error in the clock configuration and when we select the option "Resolve clock issue Automatically" then the Clock becomes 120 MHz. Don't this protocol work in lower frequency?

In addition to that , I need to use SPI and FSMC in the same controller. Whether any issue will arise in future? Can anybody help me?

    This topic has been closed for replies.

    5 replies

    TDK
    August 2, 2023

    USB requires a reliable 48 MHz clock. You can typically use a PLL to generate this from common crystal frequencies.

    Using SPI, FSMC and USB together poses no issues. SPI and FSMC clocks do not need to be exact unlike the USB.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Abin
    AbinAuthor
    Associate III
    August 3, 2023

    Thank You So Much for your reply! I will check this.