Setup application STM32F7508-DK to boot from qspi
Hi,
I'm new to STM32 development board and I have an STM32F7508-DK board. I have spent days trying to have a working setup in order to have a project that makes the STM32F750 boot from the QSPI flash of the board. I have been watching youtube video and readind the AN5188 which I understood (at least the concept) but when it's time to be practical it is an other story. I also had a look at the various example from the STM32Cube_FW_F7_V1.15.0 but it seems that none of those examples have been written for STM32Cubeide ! What I have try so far is to burn various loader in the internal flash of the MCU but none of them actually seems to boot the application that is flashed in qspi flash of the board. I have a couple of questions :
- Is it possible to debug an application that is executing from the qspi flash with the debugger of STM32CubeIde ? If yes what is the procedure ?
- Is there any STM32CubeIde (1.1.0) project template for application running from the qspi flash for the STM32F7508-DK board ?
Thanks