Skip to main content
chriskuku
Senior II
November 26, 2022
Question

setting A15 in GPIOA->ODR (STM32F103C8T6)

I'm pulling my hair because in a GPIO->ODR = 0x7fff bit A15 is not going down to 0. At least cannot trigger it with the negative slope in pulseview/ (sigrok FX2 LA).

A0-A3 are already programmed as outputs. This is the code in STM32CubeIDE:

static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(ON_BOARD_LED_GPIO_Port, ON_BOARD_LED_Pin, GPIO_PIN_SET);
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
 |GPIO_PIN_15, GPIO_PIN_SET);
 
 /*Configure GPIO pin : ON_BOARD_LED_Pin */
 GPIO_InitStruct.Pin = ON_BOARD_LED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(ON_BOARD_LED_GPIO_Port, &GPIO_InitStruct);
 
 /*Configure GPIO pins : PA0 PA1 PA2 PA3 */
 GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /*Configure GPIO pins : PB10 PB11 PB12 PB13
 PB14 PB15 PB8 PB9 */
 GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12|GPIO_PIN_13
 |GPIO_PIN_14|GPIO_PIN_15|GPIO_PIN_8|GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /*Configure GPIO pin : PA15 */
 GPIO_InitStruct.Pin = GPIO_PIN_15;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
}

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
November 26, 2022
chriskuku
chriskukuAuthor
Senior II
November 26, 2022

Oh man. Good to know it's a gotcha and not my ignorance. or inability :) So PA12 would worlk then instead?

waclawek.jan
Super User
November 27, 2022

Probably yes.

JW