RUN/Debug configuration & toolbar buttons with STM32CubeIDE
Before STM32CubeIDE, I used AC6 SystemWorkbench IDE. I had no problems with the run and debug configuration for STM32 MCU C/C++ Applications.
On STM32CubeIDE, I don't get the run button in the toolbar nor the run command in the RUN drop-down menu ( I only tested Linux and OSX versions, I can see on some video tutorials that this problem doesn't seem to be present on windows 10 versions). I don't have any problem with the debug function which is present both on the toolbar and in the RUN drop-down menu.
If I use the CTRL + F11 shortcut, debug works fine, whereas the Shift + CTRL + F11 shortcut (RUN) only rebuilds and then stops. I deduced that the button and the command in the drop-down menu are not present because the run functionality is somewhere disabled.
I thought that it might be a missing running/debug configuration for the RUN command, but It seems that only one run configuration is used for both run and debug (That's the way it is on SW4STM32 if I understand correctly the settings)
Is there some manual configuration to do when using STM32CubeIDE on Linux or OSX ?
Thanks,
Vincent.