RTOS use Taskhandle in other .c file
Hello guys,
i try to use RTOS with my STM32H723, but i have some trouble with the RTOS Tasks and the proper definition of the task.
As an example i want to push the blue button on my Nucleo board, which triggers an Interrupt, which executes a RTOS Task (https://www.freertos.org/taskresumefromisr.html)
When you create a RTOS Task in CubeMX the IDE generates the following code in the main.c file:
/* Definitions for BlueButton */
osThreadId_t BlueButtonHandle;
const osThreadAttr_t BlueButton_attributes = {
.name = "BlueButton",
.stack_size = 128 * 4,
.priority = (osPriority_t) osPriorityHigh,
};The interrupt handler functions, that I want to use, are in the stm32H/xx_it.c file.
In this file I have the following IRQ handler:
void EXTI15_10_IRQHandler(void)
{
/* USER CODE BEGIN EXTI15_10_IRQn 0 */
if(__HAL_GPIO_EXTI_GET_FLAG(BLUE_BUTTON_Pin))
{
BaseType_t checkIfYieldRequired;
checkIfYieldRequired = xTaskResumeFromISR(BlueButtonHandle);
portYIELD_FROM_ISR(checkIfYieldRequired);
//Blink_LEDs();
}
/* USER CODE END EXTI15_10_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(BLUE_BUTTON_Pin);
/* USER CODE BEGIN EXTI15_10_IRQn 1 */
/* USER CODE END EXTI15_10_IRQn 1 */
}But obviously the "BlueButtonHandle" is not declared in the _it.c file.
Since I am a beginner to c++ programming I cant figure out how to properly define the TaskHandler in my header file.
When I copy the IRQ Handler in my main.c file, everything works fine, but this is not a good solution.
Can someone help me with this problem?
Best regards,
Dennis