Skip to main content
awiernie
Associate III
July 28, 2021
Solved

RTOS support improvements: full call stack for all tasks in the Debug view

The most recent update of STM32CubeIDE says:

" RTOS support improvements: full call stack for all tasks in the Debug view"

I have installed STM32CubeIDE 1.7.0 but cannot see any difference. In the debug view (on the left) I see only Thread #1, which refers to one of the rtos threads depending which thread was active. In the "FreeRTOS task list" however, the tasks are shown (which was also true before the update). Are there additional steps necessary?

This topic has been closed for replies.
Cartu38 OpenDev
Cartu38 OpenDevBest answer
Graduate II
July 28, 2021

3 replies

Cartu38 OpenDev
Cartu38 OpenDevBest answer
Graduate II
July 28, 2021
NRoos.1348
Associate II
August 19, 2021

And in INC/FreeRTOSConfig.h, set configUSE_PORT_OPTIMISED_TASK_SELECTION to 0.

awiernie
awiernieAuthor
Associate III
August 19, 2021

The hint from Cartu38 reading the new manual section 6.3 had helped. The modification with configUSE_PORT_OPTIMISED_TASK_SELECTION was already part of subsection 6.3.