Skip to main content
TJack.2
Associate III
Dec 18, 2024 11:34 AM UTC
Question

Reverting CubeIDE to previous version (solved)

Having upgraded CubeIDE to version 1.17.0 using 'check for updates' and found it didn't work for my project, I tried to go back to version 1.15.1 using the revert button.  After running this, the IDE would not start and give an error message indicating that the ~/.eclipse/com.st.stm32cube.ide.mcu.rcp.product_1.15.1_139064214_linux_gtk_x86_64/configuration/config.ini file had blank filenames.  I found what looked like a complete file at /opt/st/stm32cubeide_1.15.1/configuration/config.ini which I copied to the above location and which then worked OK.

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
Dec 18, 2024 11:37 AM UTC

Hello @TJack.2 ,

Better to ask a question / describe the issue then add a comment where you provide the solution and accept it as solution.

Thanks

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.