Skip to main content
Associate II
Jan 22, 2025 9:28 AM UTC
Question

Request for old stm32cubeIDE versions 1.14.0 and 1.15.0

Hi ST Community,

I am using the board of STM32WBA55CGU6 board for OTA application and i want to use the application present in STM32Cube_FW_WBA_V1.3.0 and STM32Cube_FW_WBA_V1.2.0 packages. Since these packages are present in STM32Cube IDE version 1.15.0 and STM32Cube IDE version 1.14.0 respectively and is not available in the community for installation, i request to send the respective files to the mail id :- " shivaparbati2001@gmail.com "

Thank You.

This topic has been closed for replies.

4 replies

Mike_ST
ST Technical Moderator
Jan 22, 2025 10:11 AM UTC

Hello,

You can download older WBA packages there:

STM32Cube MCU Package for STM32WBA github 

Select "Tags" instead of "Branches", choose the version and download zip.

 

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
ShakuAuthor
Associate II
Jan 22, 2025 10:30 AM UTC

Thank you 

But i have the packages but i want the IDEs (stm32cubeIDE versions 1.14.0 and 1.15.0) as it is not available in ST Community. Please provide the IDEs files.

Peter BENSCH
ST Technical Moderator
Jan 22, 2025 10:34 AM UTC

@Shaku Newer versions of STM32CubeIDE can work with older firmware versions, but not vice versa. You can and should therefore use the latest STM32CubeIDE and then install the desired firmware version.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ShakuAuthor
Associate II
Jan 22, 2025 10:41 AM UTC

Thank You

After installing the newer version of the IDE the older version's packages are unable to select and unable to use and giving errors regarding errors after compilation.