Skip to main content
mmalex
Associate II
December 1, 2019
Question

request: board examples using the CubeIDE project structure

When stumped, I've found that the examples in the various board zip files that STMCubeIDE downloads are very helpful. However none of them are structured in a way that I know how to load into the 'modern' STM32CubeIDE. is there any documentation aimed at a new user of the STM32CubeIDE ecosystem, wanting to compile or modify or run the example code? the readme.txt seems to refer to keil and other IDEs I am not familiar with.

a 'quick start guide to getting the samples running' from the POV of someone who has bought a nucleo board and download STM32CubeIDE as their first (and only) STM IDE would be enormously helpful.

For now, I've got used to generating a new blank project using the IDE, then copying bits of the initialization code from the example, scattering the bits into the various c files in the IDE generated project. But there must be an easier way....?

thanks

This topic has been closed for replies.

1 reply

S.Ma
Principal
December 1, 2019

Maybe the examples were built before CubeMX and as there are significant amount of examples, migration might take some time...

I would guess coming soon in new STM32 families?