Skip to main content
LMorr.3
Senior
April 13, 2022
Question

Renaming a SMT32CubeIDE project.

I have a project folder named 'myProject' on my hard drive. I want to rename it to 'myProjectOld'. How do I do this in SMT32CubeIDE? I tried using the 'rename' function however it only renames the project in SMT32CubeIDE and not the directory on the hard drive. If I delete 'myProject' from my workspace, close SMT32CubeIDE, rename my directory to 'myProjectOld', and try to 'import' it back into SMT32CubeIDE, nothing happens. It does not appear in my workspace and I see no message of any kind.

Any ideas?

This topic has been closed for replies.

2 replies

LMorr.3
LMorr.3Author
Senior
April 13, 2022

Update: I was able to rename a project by first using the 'rename' feature in SMT32CubeIDE to rename it to 'myProjectOld', and I then 'deleted' that project from the workspace. ( kept files on local drive ) I closed SMT32CubeIDE and renamed the directory to 'myProjectOld'. I opened SMT32CubeIDE and used the 'import' feature to load my renamed project into my workspace as 'myProjectOld'. I was able to create a new project named 'myProject'.

Not sure if this is the correct way to rename.

Pavel A.
April 13, 2022

Yes, this is one of correct ways to rename. Should be safe.

Closing CubeIDE is not required when the project is closed and unloaded.