Skip to main content
Associate
Mar 22, 2025 12:29 PM UTC
Question

Received Data length is wrong in usb Communication

"static uint8_t USBD_CDC_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum)"

In stm32u575 controller and in this function while I am calling

"uint32_t receivedLength = USBD_LL_GetRxDataSize(pdev, epnum);" it gives me 1 insted of 6 or 5 bytes I am reciving so that I could not get entire data

 

This topic has been closed for replies.

3 replies

TDK
Mar 22, 2025 2:00 PM UTC

Probably the data is being split up into several packets. What program is sending the data?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Sarathk3kAuthor
Associate
Mar 24, 2025 6:19 AM UTC

It is a company software.We have to communicate with that.

void HAL_PCD_IRQHandler(PCD_HandleTypeDef *hpcd)

In this function ep->xfer_count += (RegVal & USB_OTG_GRXSTSP_BCNT) >> 4;  the xfer_count becomes 1 instead of 6 bytes or 5 bytes we are receiving. If I forcefully put it into 6 .I will get the first entire string.