Skip to main content
Associate
May 28, 2025 8:50 PM UTC
Question

RC Receiver input not being picked up

 

Screenshot 2025-05-28 at 22.46.07.png

This is the code i am using to pick up input from RC receiver to then change pwm values, but there seems to be a problem. PWM's are unresponsive to RC receiver which is connected to timer 2 channels. Is the given code correct? could it be that HAL_Delay is causing problems? I would appreciate any feedback, ive spent too much time trying to figure out the issue. 

 

 

This topic has been closed for replies.

2 replies

Pavel A.
May 28, 2025 8:58 PM UTC

What if you change batteries into the transmitter thing? Just guessing.

 

SonzayeAuthor
Associate
May 29, 2025 6:46 AM UTC

The transmitter works perfectly fine actually, the problem is that i think ic_width stays empty, i cant check too because the ports for uart 2 are being used for timer and there are no other 5v resistant ports i can put the timer on.