Skip to main content
Associate II
Sep 5, 2025 6:04 AM UTC
Question

python script in STM32CubeIDE

How to add a python script to introduce build errors during compilation process when some of the GPIO settings are modified from the below ones. PFB the python script

import sys
import re
# ‌‌ Define the locked GPIO settings here
LOCKED_SETTINGS = {
# Format: "PinName.Property": "ExpectedValue"
"PA0.GPIO_Label": "Button1",
"PA0.GPIO_Mode": "GPIO_MODE_INPUT",
"PA0.GPIO_PuPd": "GPIO_NOPULL",

"PB5.GPIO_Label": "LED1",
"PB5.GPIO_Mode": "GPIO_MODE_OUTPUT_PP",
"PB5.GPIO_PuPd": "GPIO_NOPULL",
"PB5.GPIO_Speed": "GPIO_SPEED_FREQ_LOW",
}
def check_ioc_file(ioc_path):
try:
with open(ioc_path, "r", encoding="utf-8") as f:
lines = f.readlines()
except FileNotFoundError:
print(f"‌‌ ERROR: File not found: {ioc_path}")
sys.exit(1)

errors = []
for key, expected_value in LOCKED_SETTINGS.items():
found = False
for line in lines:
if line.startswith(key + "="):
found = True
actual_value = line.strip().split("=")[1]
if actual_value != expected_value:
errors.append(f"{key} changed! Expected '{expected_value}', found '{actual_value}'")
break
if not found:
errors.append(f"{key} missing from {ioc_path}")

if errors:
print("‌‌ GPIO lock check failed:")
for err in errors:
print(" - " + err)
sys.exit(1)
else:
print("‌‌ GPIO lock check passed.")

if __name__ == "__main__":
if len(sys.argv) != 2:
print("Usage: python check_ioc_lock.py Temp-STM32H743VIHX.ioc")
sys.exit(1)
check_ioc_file(sys.argv[1])

Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.

1 reply

Ghofrane GSOURI
ST Technical Moderator
Sep 12, 2025 9:16 AM UTC

Hello @GHM 

STM32CubeIDE supports running Python scripts in the Pre-build and Post-build steps, provided that Python is installed and accessible in your system’s PATH. To enforce GPIO configuration checks, place your check_ioc_lock.py script and your .ioc file in the project root directory. Then, in the IDE, right-click your project, select Properties ==> C/C++ Build ==> Settings ==> Build Steps, and enter the appropriate command to execute your Python script (e.g., python check_ioc_lock.py Temp-STM32H743VIHX.ioc) in the Pre-build steps field. This setup ensures that your script runs automatically before each build.

GhofraneGSOURI_0-1757668559779.png

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.