Skip to main content
SKape
Associate II
Dec 1, 2023 6:14 AM UTC
Question

$PWD returns an empty string when called from STMCubeIDE 1.14.0

Hello.

I found one more problem with the latest version of STM32CubeIDE 1.14.0
I am using STM32CubeIDE under Windows 7
I have the latest "git for Windows" installed, which provides me with a bash console. The directory with the bash command is added to the system path.
Before compilation, I run a bash script that obtains data from GIT and places it in the header file.
The script is run with the "bash prebuild.sh" command entered in Pre-build steps in the project properties.
The script works correctly if run directly from the bash console or the previous version of STMCubeIDE 1.13.2
If it is called from the latest version of STMCubeIDE 1.14.0, the $PWD variable or the pwd command in the script return an empty string instead of the current path.
What could be the problem with this behavior?

    This topic has been closed for replies.

    7 replies

    Peter BENSCH
    ST Technical Moderator
    Dec 1, 2023 9:40 AM UTC

    I would like to point out that STM32CubeIDE 1.14.0 no longer supports Windows 7, which can also be found in the release notes RN0114, section 1.2:

    Supported operating systems and architectures

    • Windows® 10 and 11, 64 bits (x64)
    • Linux®: Ubuntu® LTS 20.04 and LTS 22.04, and Fedora® 36
    • macOS® 12 (Monterey), macOS® 13 (Ventura)

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    awiernie
    Associate III
    Dec 18, 2023 11:58 PM UTC

    I have the same problem on Windows 11, see below.

    fronders
    Associate III
    Dec 4, 2023 11:53 AM UTC

    @Peter BENSCH Hi :)
    I too have a similar problem with pre-build & post-build scripts, on Windows 10 x64 with the latest BusyBox v1.31.0.st_20231030-1215 & included make tools with CubeIDE v1.14.0 (plugin com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.100.202310302056).

    It used to work okay on CubeIDE v1.13.2 which included BusyBox v1.31.0.st_20200221-0903_longpath (plugin com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.0.202305091550). 


    I'm experiencing problems not only with the $PWD outputting blank line.
    mv command fails with 'Result too large' in a pre-build script. 

     

    Here is the script (added some prints for debugging):

     

     

    #!/bin/bash -
    # prebuild script
    
    # update git version and build timestamp
    versionfile="../Inc/git_version.h"
    version_git=`git describe --dirty --always`
    echo "git version: \"$version_git\""
    echo "#define GIT_VERSION \"$version_git\"" > tempver
    build_time=`date +"%Y-%b-%d %T"`
    echo "build time: \"$build_time\""
    echo "#define BUILD_TIME \"$build_time\"" >> tempver
    
    
    echo ""
    echo "PWD output: $PWD"
    echo ""
    echo "tempver file:"
    ls -l tempver && cat tempver
    echo ""
    echo "versionfile:"
    ls -l $versionfile && cat $versionfile
    echo ""
    
    if cmp -s tempver $versionfile
    then
     rm tempver
    else
     mv tempver $versionfile
    fi
    
    exit 0

     

     

     

    This is the output, you can see paths to files resolve okay, and the access rights are also okay, their content is printed, but mv fails:

     

     

    13:33:17 **** Incremental Build of configuration Debug for project app_test ****
    make -j8 all
    "../prebuild.sh"
    git version: "g9cee9c1-dirty"
    build time: "2023-Dec-04 13:38:09"
    
    PWD output:
    
    tempver file:
    -rw-rw-r-- 1 alexa alexa 91 Dec 04 13:38 tempver
    #define GIT_VERSION "g9cee9c1-dirty"
    #define BUILD_TIME "2023-Dec-04 13:38:09"
    
    versionfile:
    -rw-rw-r-- 1 alexa alexa 79 Dec 03 11:25 ../Inc/git_version.h
    #define GIT_VERSION "g9cd0444-dirty"
    #define BUILD_TIME "2023-Dec-03 11:25:53"
    
    mv: can't rename 'tempver': Result too large
    
    make[1]: Nothing to be done for 'main-build'.

     

     

     

    If I replace the busybox binaries to older ones from CubeIDE v1.13.2 everything is back to normal and mv is successful

     

    13:55:37 **** Incremental Build of configuration Debug for project app_test ****
    make -j8 all 
    "../prebuild.sh"
    git version: "g9cee9c1-dirty"
    build time: "2023-Dec-04 13:55:40"
    
    PWD output: C:/Users/alexa/Repo/app_test/Debug
    
    tempver file:
    -rw-rw-r-- 1 alexa alexa 91 Dec 04 13:55 tempver
    #define GIT_VERSION "od_v0.101-5-g9cee9c1-dirty"
    #define BUILD_TIME "2023-Dec-04 13:55:40"
    
    cat versionfile:
    -rw-rw-r-- 1 alexa alexa 79 Dec 03 11:25 ../Inc/git_version.h
    #define GIT_VERSION "g9cd0444-dirty"
    #define BUILD_TIME "2023-Dec-03 11:25:53"
    
    ... rest of the build logs (compiler etc)

     

     

    awiernie
    Associate III
    Dec 18, 2023 11:57 PM UTC

    I have the same problem after updating to STM32CubeIDE 1.14 (on Windows 11).

    I have a postbuild.sh which has lines wich should get the working directory like this:

    current_directory=`pwd`

    This is empty. 

    $pwd delivers also an empty string.

     

    Ernst

    awiernie
    Associate III
    Dec 19, 2023 12:27 AM UTC

    I have now 2 external tools subdirectories. Is it possible to select it somewhere in the IDE/or project settings in order not to have to reinstall the old STM32CubeIDE?

    Rim LANDOLSI
    ST Employee
    Dec 19, 2023 2:37 PM UTC

    Hello and welcome to the community,  

     

    Thank you for your contributions, the issue is related to busybox binaries.  An internal ticket ID 167912(This is an internal tracking number and is not accessible or usable by customers) has already been submitted to escalate this issue internally to the STM32CubeIDE team.

     

    Thanks,

    Rim

    fronders
    Associate III
    Jan 23, 2024 1:45 PM UTC

    Hello @Rim LANDOLSI,

    this issue seems to be addressed in CubeIDE v1.14.1 patch and that indeed fixed the $PWD being empty and mv spitting out "Result too large" error.

     

    However, after updating to v1.14.1 the mv command keeps failing but with a different error now:

    echo "test" > tempobj
    mv -f tempobj "test.txt"
    test -f tempobj && cat tempobj || echo "no tempobj file"
    test -f "test.txt" && cat "test.txt" || echo "no test.txt file"

    runs okay the first time:

    15:41:29 **** Incremental Build of configuration Debug for project test ****
    make -j8 all 
    bash ../prebuild.sh
    no tempobj file
    test 
    
    arm-none-eabi-gcc ...
    ...

    but gives an error on the next ones (because test.txt already exists):

    15:42:59 **** Incremental Build of configuration Debug for project test ****
    make -j8 all 
    bash ../prebuild.sh
    mv: can't rename 'tempobj'
    test
    test
     
    arm-none-eabi-gcc ...
    ...

    Using mv -f does not help either.

    So far I have been able to "hack" all my mv commands with cp+rm which kinda solves the issue, so the prebuild script at least works, but this needs to be addressed and fixed