Skip to main content
Associate III
Jul 14, 2025 3:50 PM UTC
Question

"project is part of hierarchical structure. Would you like to import entire project structure?"

Hi,

After CubeMX auto-code generation, CubeIDE shows message: " project XXX is part of hierarchical structure. Would you like to import entire project structure? Yes/NO?  "

if I choose "Yes", a sub-directory will be created inside my project which is not desirable. How to fix it?

Thanks,

Peter

This topic has been closed for replies.

2 replies

ST Technical Moderator
Jul 14, 2025 4:30 PM UTC

Hello @RongShengWang 

Ensure that the project is not generated inside another project and try to change the path of your project to another directory.

BR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate III
Jul 16, 2025 4:02 PM UTC

I had to check "Generate under root" checkbox in Project Manager". I did not, which wasted me 3 days to deal with many troubles caused by the simply clicking the checkbox. It should be defaulted to  "Generate under root"