Project imported from TouchGFX but not able to debug for board STM32H745I - DISCO
- 3 replies
- 1323 views
Board : STM32H745I - DISCO
Cubeide : v.1.13.2
TouchGFX : v4.22.1 Designer
STM32H745I - DISCO as it is dual core m4 and m7
1st i did build and debugging for m4 processor. It is successful.
2nly done with building for m7 processor.It is successful
But while debugging the m7 i am facing following issue ??????
please help me with this .
Error in final launch sequence:
Failed to execute MI command:
load C:\\TouchGFXProjects\\11092023\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\11092023\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\11092023\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf
Error message from debugger back end:
Load failed
Load failed