Skip to main content
ANauz.1
Senior
Mar 22, 2022 10:23 AM UTC
Solved

Project importation not working with STM32CubeIDE v1.9.0

Hello,

I was working with STM32CubeIDE version 1.8.0 on a project. I just download version 1.9.0, trying to import the project.

In the importation Wizard, when selecting the correct directory, the project name is displayed, but when clicking "Finish", the importation window close, and nothing append.

Is this a known issue? Is there something to do to make it work?

Thank you

Antoine

ANauz.1
ANauz.1Best answer
Senior
Mar 29, 2022 12:33 PM UTC

Hello,

I finally managed to import the project.

The problem was that I selected as new workspace, the project directory, and that is not possible.

But there was no error messages displayed.

Selecting another WS directory solve the issue. But message should be displayed.

I was trying to import using "File->Open project from file system"

4 replies

Markus GIRDLAND
ST Employee
Mar 24, 2022 8:06 AM UTC

Hello there!

Could you give some additional details about what options you use in order to import? Along with some screenshots of the process?

It's also important to note that it's recommended to have a new workspace for STM32CubeIDE 1.9.0 and then import the old project into the new workspace.

ANauz.1
ANauz.1AuthorBest answer
Senior
Mar 29, 2022 12:33 PM UTC

Hello,

I finally managed to import the project.

The problem was that I selected as new workspace, the project directory, and that is not possible.

But there was no error messages displayed.

Selecting another WS directory solve the issue. But message should be displayed.

I was trying to import using "File->Open project from file system"

ABans.3
Associate II
Oct 17, 2024 1:59 PM UTC

@ANauz.1 Yeah I wasted about and hour to figure out this. It should show that it cannot configure the project on this folder workspace.

In my experiment, you also cannot import a project into the workspace if project folder is direct child of workspace or viceversa

MichaelDevine
Associate II
Apr 26, 2026 6:18 AM UTC

This issue has regressed. I am not able to import projects that I just set up with CubeMX. Here are the steps:

1. Open CubeMX, enter my board, click on an example, set the path and save it. 

2. Open STM32CubeIDE, opening the parent folder of the project. Choose import, select the folder the project is in, it successfully finds the project so then I click Finish3.
3. Then, nothing! No error, and no projects added to the workspace. 

Screenshot 2026-04-25 231523.png