Skip to main content
SKled.1
Senior
April 30, 2024
Question

Project explorer highlighting .ld files - how to stop that?

No idea with what version that came, just updated to 1.15.1 after a couple months, and linker scripts are now written in bold font.
Kinda arbitary, needlessly distracting and annoying. I know what files I find important when, don't need a nanny for that, okay?

How do I disable that?

-

EDIT:

While we're at it, the update to 1.15 did annoying things additional to the above:

  1. installed a toolchain (gcc12) I did not ask for, wasting space AND
  2. break existing toolchain settings for some of the installed compilers, which forced me to "add manually" in toolchain manager, the one that's still on the system but somehow CubeIDE forgot about, so the projects won't all light up red and claim their toolchain doesn't exist.
  3. Put an icon into the text menu bar (seriously, WTF?), making it stand out there as the most important item, i.e. the "myST" login, which I will never use & is defacto the very least important item, whether you greedy data grabbers think so or not, in fact, this doesn't belong in an IDE at all, how about copying those things from Visual Studio that enhance productive functionality instead of such ***? Another utterly annoying distraction, next to the bold font linkerscripts. [not 100% sure it was this or prev update, wasn't using the IDE much for the past couple updates]
This topic has been closed for replies.

2 replies

Andrew Neil
Super User
April 30, 2024

@SKled.1 wrote:

No idea with what version that came


Not doing it in 1.13.0

Does seem pointless and unnecessary - just a distraction.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
Super User
April 30, 2024

I had IDE 1.13.1 and now using  1.14.1 - no problems.

So try 1.14.1 - maybe your "problem" solved. (But i dont know...so up to you.)

If you feel a post has answered your question, please click on " Best Answer ".