Skip to main content
Peeters.Bram
Associate III
Nov 6, 2020 10:56 AM UTC
Solved

Processor peripheral registers view missing ?

Hi,

I am trying out the cubeide coming from IAR. I am currently having a problem that some interrupt is occuring which goes to the default handler. Since all unmapped interrupt functions go to the same handler apparently CubeIDE shows an incorrect interrupt as entry point. So I am trying to figure out which interrupt is really occurring. I thought I would go to the register view and look op the nvic registers but it turns out that this register view is only showing some core registers and not the peripheral registers (stm32f7). Can I find them somewhere else ? Other suggestions ? Worst case, is there an (easy) way to add them myself ?

This topic has been closed for replies.
Peeters.Bram
Peeters.BramBest answer
Associate III
Nov 6, 2020 11:21 AM UTC

Ok , apparently cubeid has a 'register view' for core registers, and a SFRs view for peripheral registers.

6 replies

Peeters.Bram
Peeters.BramAuthorBest answer
Associate III
Nov 6, 2020 11:21 AM UTC

Ok , apparently cubeid has a 'register view' for core registers, and a SFRs view for peripheral registers.

Cartu38 OpenDev
Graduate II
Nov 6, 2020 1:25 PM UTC

If your issue is solved please tag as answered ... will help community

Peeters.Bram
Associate III
Nov 9, 2020 4:06 PM UTC

What exactly does 'tag as answered' means. I do not immediately see a way to change the status of this question to solved or something.

LaurentL
ST Employee
Nov 23, 2020 10:09 AM UTC

Hi,

In STM32CubeIde v1.5.0, the core registers have been added with the peripheral registers in the same SFRs view.

Rgds,

Laurent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Peeters.Bram
Associate III
Dec 15, 2020 12:33 PM UTC

Hi Laurent,

I recently upgraded to 1.5.0, but the R0/R1/.... registers are still in a different view as the peripheral registers ?

Or what do you call core registers ?

I am working with a cortex M7

Regards

Bram

LaurentL
ST Employee
Dec 15, 2020 1:11 PM UTC

Hello,

In v1.5.0, the core registers have been added with peripheral registers, so now you can see the NVIC, MPU, Systick...registers in the same view.

The General registers have not been modified, all R0-Rx, SP, LR, PC and FPU regs are in this view.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.