Skip to main content
Associate
December 20, 2023
Question

Problem with remore target debugging in cubeide 14

I have problems with remote debugging of an STM32L432 device from STM cube ide ver 1.9 on arch linux.g

I can connect and debug with cube with the target directly connected.

When i connect to a remote raspberry with the same tarrgeti i get an error: "Could not verify ST device".
In the gdb log in stmcube i get the following:

 

877,561 &"monitor ReadAPEx 0x0 0xF8\n"

877,566 @"invalid command name \"ReadAPEx\"\n"

877,567 &"Protocol error with Rcmd\n"

877,567 24^error,msg="Protocol error with Rcmd"

it seems ReadAPEx command is unavalible.

Debugging with cli-gdb seem to work, but has no ReadAPEx instruction.

I can connect with an old version of stmcube on windows platform, but this version does not seem to send the ReadAPEx command.

I have tried openocd version 0.12 and pyocd 0.36 on the raspberry and result is the same with both servers.
st-util 1.7 is not working, neither with new or old cube.

 

Anyone experienced the same thing? I found some thread about mod_cmd_extended.cfg but this files seem to be non-existing on all my stm32 installations.

 

 

This topic has been closed for replies.

2 replies

Visitor II
July 19, 2024

Me too with a different target STM32F103ZCHx

Did you get anywhere?

 

/Peter

pejjoAuthor
Associate
August 12, 2024

Unfortionately not.

I ended up with installing VirtualHere USB driver and thus "moving" the port to the IDE machine.

Anoying, but couldnt find any other solution.