Skip to main content
Associate III
December 1, 2023
Question

PROBLEM WITH POSIX

Hi all,Ihave a project on stm32cubeide and I use threadx in mu nucleo-144-u575zi-q .I 've  used PTHREAD_ONCE_INIT and put  #include <tx_opsix.h> in my code but the compiler not found that file. I found it in C:\Users\Roberto\STM32Cube\Repository\STM32Cube_FW_U5_V1.3.0\Middlewares\ST\threadx\utility\rtos_compatibility_layers\posix\ so I open the window "project/properties/path&symbol/includes and I 've added this path from the voice "filesystem" because in my workspace in C:\Users\Roberto\STM32Cube\Repository\STM32Cube_FW_U5_V1.3.0\Middlewares\ST\threadx\utility\rtos_compatibility_layers\ path there is only "low_power" folder and not "posix"(WHY?).

The compiler found tx_posix.h now but it give me this error : 

In file included from ../Core/ThreadSafe/newlib_lock_glue.c:66:

../Core/ThreadSafe/newlib_lock_glue.c: In function '__retarget_lock_init_recursive':

C:/Users/Roberto/STM32Cube/Repository/STM32Cube_FW_U5_V1.3.0/Middlewares/ST/threadx/utility/rtos_compatibility_layers/posix/errno.h:52:15: error: 'posix_errno' undeclared (first use in this function)

52 | #define errno posix_errno

| ^~~~~~~~~~~

../Core/ThreadSafe/newlib_lock_glue.c:126:5: note: in expansion of macro 'errno'

126 | errno = EINVAL;

| ^~~~~

C:/Users/Roberto/STM32Cube/Repository/STM32Cube_FW_U5_V1.3.0/Middlewares/ST/threadx/utility/rtos_compatibility_layers/posix/errno.h:52:15: note: each undeclared identifier is reported only once for each function it appears in

52 | #define errno posix_errno

| ^~~~~~~~~~~

../Core/ThreadSafe/newlib_lock_glue.c:126:5: note: in expansion of macro 'errno'

126 | errno = EINVAL;

| ^~~~~

make: *** [Core/ThreadSafe/subdir.mk:19: Core/ThreadSafe/newlib_lock_glue.o] Error 1

make: *** Waiting for unfinished jobs....

"make -j8 all" terminated with exit code 2. Build might be incomplete.

 

17:40:09 Build Failed. 3 errors, 24 warnings. (took 15s.422ms)

 

Someone can help me?

 

Thanks in advances

 

 

 

because in workstation (despite at beginning of project I've select "THREADX" and I have AZURE_RTOS and 

This topic has been closed for replies.