Problem with NUCLEO-H743ZI2 and STM32CubeIDE debugging
- 4 replies
- 1990 views
Hello,
I have recently bought the NUCLEO-H743ZI2 board and I can't use the on board STLINKV3 debugger with STM32CubeIDE, in ST-LINK GDB Server mode. However I can debug in OpenOCD mode.
The error I get is the following:
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: C:\Users\grag\AppData\Local\Temp\STM32CubeProgrammer_a10060.log
ST-Link Server is running on port : 7184
ST-LINK SN : 002B00293137510939383538
ST-LINK FW : V3J2M1
Voltage : 3.28V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a10060.srec
File : ST-LINK_GDB_server_a10060.srec
Size : 18356 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.050
Verifying ...
Download verified successfully
Target unknown error 19
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
Failed to restart ST-LINK connection
Error in STM32CubeProgrammer
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Debugger connection lost.
Shutting down...
Does anybody know what to look?
Attached is the log file from the debugger.
Best Regards,
Ioannis Gragopoulos