Skip to main content
GHrib.1
Associate III
February 20, 2023
Question

Problem with memcpy

Hello,

I am having a problem with simple line of code. If I run code bellow, the result seems off.

//Main job of this code is to tranform hex into float 
 
uint32_t hex = 0x3fc51eb8;
float f;
 
memcpy(&f, &hex, 4);

If i go into Live Expressions i get that f = 0x1 (hex), it should be f = 0x3fc51eb8. The strangest thing is that the same code works for example on an onlineGDB compiler.

I assumed the trouble was within compiler, therefore I tried to change from default GNU 11 to some others, but there were no change. Any idea what could be wrong?

I am using:

NUCLEO G474

cubeIDE Version: 1.10.1 Build: 12716_20220707_0928 (UTC)

This topic has been closed for replies.

2 replies

GHrib.1
GHrib.1Author
Associate III
February 20, 2023

I found out that everything works fine except maybe cubeIDE (Number format option in debug perspective). The problem is that there is something wrong with hex Number format. If the number format is set as Default, then floats have correct values. Is there a bug inside cubeIDE or do I not understand what does Number format option do.

I added another variable (float test = 5.3) inside the code from previous post. By changing Number format option i get.

  • Default (values are ok):

0693W00000aHF2UQAW.png 

  • Hex (only hex variable is correct):

0693W00000aHF2eQAG.png 

  • Decimal(only hex variable is correct):

0693W00000aHF2tQAG.pngIs this kind of behavior anticipated?

Tesla DeLorean
Guru
February 20, 2023

Seems unhelpful, but 1.54 probably doesn't print well as the actual number, in hex.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..