Skip to main content
JimEno
Associate III
Sep 18, 2025 3:01 PM UTC
Solved

Problem with LwIP_TCP_Echo_Server on Nucleo-H7S3L8 Eval Board

Firstly, the installation process is pretty ugly and the documentation is very sparse.

From the README.md file:

This application runs from the external Flash memory (LwIP_TCP_Echo_Server Appli).

It boots from internal Flash (Template_XIP_Boot) then jumps to the application code in external Flash.

To configure STM32CubeIDE Debug Configuration, you must do the following :

 

1. Upload the template XIP

2. Add the adequate external loader (MX25UW25645G_STM32H7S3L8-NUCLEO.stldr file) in Project->Debugger Configuration

3. Add in the startup the template_XIP_Boot in Project->Debugger Configuration

4. Move up the application in the startup

 

Step 1, real helpful, what an ordeal.

Step 2, could not find MX25UW25645G_STM32H7S3L8-NUCLEO.stldr used MX25UW25645G_NUCLEO-H7S3L8.stldr instead

Environment:

STMCubeIDE V1.19.0

STMCubeMX V6.15

STMProgrammer V2.20.0

ST-Link F/W V3J16M9

 

My problem:

When I run the code in debugger mode, execution never gets out of Template_XIP_Boot.

Ends up in error handler.

void Error_Handler(void)

{

/* USER CODE BEGIN Error_Handler_Debug */

/* User can add his own implementation to report the HAL error return state */

__disable_irq();

while(1)

{

}

/* USER CODE END Error_Handler_Debug */

}

Call stack:

HAL_XSPI_Command returns with status=HAL_BUSY

JimEno_0-1758207067468.png

I'm sure I'm missing something but can't afford weeks to find it. Any help or insight would be appreciated.

This topic has been closed for replies.
ST Technical Moderator
Sep 30, 2025 1:35 PM UTC

Hello @JimEno ,

 

It is mentioned on the Readme file to enable high-speed option byte with STM32CubeProgrammer Tool.

XSPI2_HSLV=1

MahmoudBenRomdhane_0-1759239310637.png

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

7 replies

ST Technical Moderator
Sep 23, 2025 11:08 AM UTC

Hello @JimEno ,

 

Let me thank you for posting.

For more investigation, I suggest please that you provide the Debugger and the Startup configuration.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JimEno
JimEnoAuthor
Associate III
Sep 24, 2025 5:52 PM UTC
 

Recommended info added. Tried to follow README.md file as best as I could.

JimEno_2-1758735999873.png

JimEno_3-1758736228144.png

 

 

 

 

 

 

 

 

JimEno
JimEnoAuthor
Associate III
Sep 29, 2025 2:06 PM UTC

Additional observations:

I added a hack 'while' delay. Code snippet below.

File: stm32h7rsxx_hal_xspi   Function: HAL_XSPI_Command    Line: 875

...

/* Wait till busy flag is reset */

status = XSPI_WaitFlagStateUntilTimeout(hxspi, HAL_XSPI_FLAG_BUSY, RESET, tickstart, Timeout);

uint32_t i = 0x00050000;

while(i--);

 

if (status == HAL_OK)

...

 

This seemed to 'fix' the problem. Code did not end up in Error_Handler.

Please continue with real fault cause and fix.

New problem surfaced:

The Application code was all 0xFFFFFFFF and jump from Boot to Application crashed (of course).

I will open a new forum post on this.

ST Technical Moderator
Sep 30, 2025 1:35 PM UTC

Hello @JimEno ,

 

It is mentioned on the Readme file to enable high-speed option byte with STM32CubeProgrammer Tool.

XSPI2_HSLV=1

MahmoudBenRomdhane_0-1759239310637.png

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JimEno
JimEnoAuthor
Associate III
Sep 30, 2025 2:04 PM UTC

I was using the IDE to build and program the sample project. I assumed the IDE or MX would handle any settings or options. I did not assume I HAD to use the Programmer to set any options. I will try this and report back.

Thanks for your response Mahmoud.

JimEno
JimEnoAuthor
Associate III
Oct 5, 2025 7:02 PM UTC

Mahmoud,

I enabled that option byte as you suggested. It worked.

- User Option Bytes requirement (with STM32CubeProgrammer tool)

- XSPI2_HSLV=1 I/O XSPIM_P2 High speed option enabled

 

It seems like setting this option could have been done in the sample project

firmware. I shouldn't need the Programmer. Am I wrong?

I will consider this issue resolved. Thanks for your response.

ST Technical Moderator
Oct 6, 2025 9:49 AM UTC

Hello @JimEno 

 

Further to your comment, the XSPI2_HSLV can be done by user code as described in RM0477 section 5.4.3 Option byte words modification / Changing option byte words. VDDIO_HSLV option bit is also required with XSPI2_HSLV.

The flash driver provides the following HAL API that can be used. 

 

/**
 * @brief Program Option bytes.
 * @param pOBInit pointer to an FLASH_OBInitStruct structure that
 * contains the configuration information for the programming.
 *
 * @note To configure any option bytes, the option lock bit OPTLOCK must be
 * cleared with the call of HAL_FLASH_OB_Unlock() function.
 * @note New option bytes configuration will be taken into account in two cases:
 * - after an option bytes launch through the call of HAL_FLASH_OB_Launch()
 * - after a power reset (BOR reset or exit from Standby/Shutdown modes)
 *
 * @retval HAL Status
 */
HAL_StatusTypeDef HAL_FLASHEx_OBProgram(const FLASH_OBProgramInitTypeDef *pOBInit)

 

  • Note 1: This API will reset the device at the end to ensure the programming of the Option byte. To avoid a recall to the API after reset, you may need to test that the value of the option bit is not set before calling this API
  • Note2: Using CubeMx you need to insert this in the code for modifying HSLV option bit into the boot project, before any configuration of XSPI2. 

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.