Skip to main content
IKuba
Visitor II
July 19, 2019
Question

Problem when CubeIDE is installed not in default folder and workspace is also not in default path

Hello!

When I install CubeIDE not in default folder and change a folder for workspace there are problems with code generation. This problem occurs with MCUs and Boards. Even if one can generate some code it is not the same code as if the programm and worspace are in default paths. And the debugger does not start...

This topic has been closed for replies.