Skip to main content
JFree.1
Associate II
Aug 4, 2021 10:21 AM UTC
Solved

Problem adding source file to STM32CubeIDE project I can add a .cpp file containing a trivial test function to the Core/Src folder, 'build' seems to process it ok but can not acces this from another source file.

Declaring external function in main.c causes no error

extern plus_one (int) ; // Causes no problem

but from within main ()

int x = plus_one (2); // causes build to fail

11:20:23 **** Incremental Build of configuration Debug for project TemplateL432KC_DMA ****

make -j4 all

arm-none-eabi-g++ "../Core/Src/tesnewfil.cpp" -mcpu=cortex-m4 -std=gnu++14 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32L432xx -c -I../Core/Inc -I../Drivers/STM32L4xx_HAL_Driver/Inc -I../Drivers/STM32L4xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32L4xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"Core/Src/tesnewfil.d" -MT"Core/Src/tesnewfil.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/tesnewfil.o"

arm-none-eabi-g++ -o "TemplateL432KC_DMA.elf" @"objects.list"  -mcpu=cortex-m4 -T"C:\STMCube\TemplateL432KC_DMA\STM32L432KCUX_FLASH.ld" --specs=nosys.specs -Wl,-Map="TemplateL432KC_DMA.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group

c:\st\stm32cubeide_1.6.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Core/Src/main.o: in function `main':

C:/STMCube/TemplateL432KC_DMA/Debug/../Core/Src/main.c:298: undefined reference to `plus_one'

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:80: TemplateL432KC_DMA.elf] Error 1

"make -j4 all" terminated with exit code 2. Build might be incomplete.

This topic has been closed for replies.
TDK
TDKBest answer
Aug 4, 2021 1:51 PM UTC

The function needs to have "C" linkage in order to be called from C. To do this, you need to encase the function definition in "extern "C"" braces.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

JFree.1
JFree.1Author
Associate II
Aug 4, 2021 10:25 AM UTC

One error above, extern declaration is of course

extern int plus_one (int) ;

TDK
TDKBest answer
Aug 4, 2021 1:51 PM UTC

The function needs to have "C" linkage in order to be called from C. To do this, you need to encase the function definition in "extern "C"" braces.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JFree.1
JFree.1Author
Associate II
Aug 4, 2021 6:21 PM UTC

Many thanks, solved.