Skip to main content
Ephraimoved
Associate III
Mar 19, 2024 5:14 PM UTC
Question

post build

Dear Sir.

I have designed a bootloader that stat from 0x8100000 , length of 40k bytes,

there is also a signature of 2 bytes 0x23,0x45, at @ 0x80f6000,

at last the runtime code that start from 0x8100000.

Is it possible to use STM32IDE's post build to make the bin or hex file 

that will include all 3 sections bootloader, signature, runtime code.

 

 

Please Advise.

 

 

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    Mar 19, 2024 5:30 PM UTC

    If you can run an executable or batch file, you can do pretty much anything you want.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..