Skip to main content
LBlea.1
Visitor II
February 2, 2021
Question

PLLRDY Flag wont set

  • February 2, 2021
  • 1 reply
  • 1286 views

Goal: Use PLL functionality on either the HSI or HSE to increase clock speed.

Problem: PLLRDY flag never sets. Enters hard fault and requires reset.

Setup: 

IDE: STM32CubeIDE

MCU: STM32F070CB

HSE: NX3225SA-12.000M-STD-CSR-1 loaded with 8pF caps.

Programmer: Chinesium J-link, chinesium ST-link. Never had a problem with either of these.

Things I have tried: 

  • Many users have stated that the flash latency must be changed before PLL turned on. I have tried manually changing to mode 0 and mode 1
  • Tried HSI and HSE as PLL source. HSE looks good on a scope. Neither work.
  • Tried erasing the chip and reflashing fresh chip with PLL code.
  • Tried many different configurations of PLL multiplier...etc. within the clock configuration tab.
  • Tried the example code straight out of the reference manual for the micro on page 732.
  • Tried two different micros
  • Tried the evaluation board and PLL worked fine up to 48MHz on there...

__HAL_RCC_PLL_ENABLE();

Bricks the program every time.

Here is my configuration code:

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
 RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
 HAL_RCC_MCOConfig(RCC_MCO, RCC_MCO1SOURCE_SYSCLK, RCC_MCODIV_1);
}

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
March 18, 2021

> Tried the evaluation board and PLL worked fine up to 48MHz on there...

Then the problem is in something which is different between the evaluation board and your board. My guess is inadequate power supply, grounding arrangement, and/or decoupling.

JW