Skip to main content
Explorer
August 21, 2023
Solved

PH3-BOOT0

Hi,

I am using STM32U585RIT6 MCU & I planned to flash the firmware through SWD and onboard debugger module (STLINK-V3MODS) through VCP.

I am having confusion in configuring the PH3-BOOT0 pin.

Should I connect it to 5V or GND.

Or shall I make it No connect.

@RomainR.  Can you pls help me on this?

Thanks in advance for any suggestions or help

    This topic has been closed for replies.
    Diane POMABIABest answer
    ST Employee
    August 21, 2023

    Hi @mkm 

    If you need to boot on the internal flash memory, this pin is set to level LOW (GND) by a pull‑down resistor.

    It is possible to put this GPIO to level HIGH to boot on the system flash memory (bootloader), by connecting  this pin to VDD.

    Regards

    Diane

    1 reply

    Diane POMABIABest answer
    ST Employee
    August 21, 2023

    Hi @mkm 

    If you need to boot on the internal flash memory, this pin is set to level LOW (GND) by a pull‑down resistor.

    It is possible to put this GPIO to level HIGH to boot on the system flash memory (bootloader), by connecting  this pin to VDD.

    Regards

    Diane