Skip to main content
Associate II
February 19, 2024
Question

Output compare mode.

Good afternoon community,
I am traying to Output compare unit on STM32F407G Discovery.  
I am configuring TIM1 and generate with global interrupt. Here is timer configuration function.
This is Callback Function.

//Callback function
void HAL_TIM_OC_DelayElapsedCallback(TIM_HandleTypeDef *htim)
{
	/*It will generate 500Hz frequency*/
	if(htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
	{
		ccr_content = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1);
		__HAL_TIM_SET_COMPARE(htim,TIM_CHANNEL_1,ccr_content+pulse1_value);
	}
}

And Timer configuration is:

static void MX_TIM1_Init(void)
{

 /* USER CODE BEGIN TIM1_Init 0 */

 /* USER CODE END TIM1_Init 0 */

 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 /* USER CODE BEGIN TIM1_Init 1 */

 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 65535;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_OC_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_TIMING;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_OC_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */

 /* USER CODE END TIM1_Init 2 */
 HAL_TIM_MspPostInit(&htim1);

}

Now what code is writes in main function? Let me know.
I want to generate 1500Hz frequency with 50% of duty cycle.
Please give the reference. I am sharing my project with you for your reference.
Which configuration are need still in this code and Can i see the output on GPIO pin or toggling LED?
You can also suggest a reference example code.
Thank you.



 

    This topic has been closed for replies.

    1 reply

    TDK
    February 19, 2024

    Generally the signal is started with HAL_TIM_PWM_Start. Adjust your pulse and period values to achieve the desired timer frequency and duty cycle.

    "If you feel a post has answered your question, please click ""Accept as Solution""."