Skip to main content
Associate
Dec 27, 2024 8:35 PM UTC
Question

NucleoH7S3L8 SPI Not Working

Dear ST Community,

I have the following issue:
I try to start a simple SPI Transmit but it seems that after a first burt of clocks which I observe on the osciloscope, the program gets stack in the Error_Handler, while it shouldn't based on .ioc configuration and the code.
I attach the respective main.c script that describes the situation:

 

//=====================================System's Code===================================
/* USER CODE BEGIN PTD */
#define BUFFER_SIZE 512
uint8_t txBuffer[BUFFER_SIZE*4];
/* USER CODE END PTD */ 
//=====================================System's Code====================================
for (uint16_t i = 0; i < BUFFER_SIZE * 4; i++) {
 txBuffer[i] = i & 0xFF;
 }
 if (HAL_SPI_Transmit(&hspi1, txBuffer, BUFFER_SIZE*4, 5000) != HAL_OK) {
 Error_Handler();
 }
 while (1)
 {

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 BSP_LED_Toggle(LD2);
	 HAL_Delay(500);
 }
 /* USER CODE END 3 */
}
//=====================================System's Code====================================
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
	 BSP_LED_Toggle(LD1);
	 HAL_Delay(50);
 }
 /* USER CODE END Error_Handler_Debug */
}
//=====================================System's Code====================================

 

 

Please let me know if you have any suggestions. Thank you!
Best Regards,
Dimitris

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Dec 27, 2024 11:08 PM UTC

What error does the function actually return? Understand that in the context of the failure. Source for the library is provided.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ghofrane GSOURI
ST Technical Moderator
Dec 31, 2024 8:54 AM UTC

Hello @DG91 

First let me thank you for posting.

Could you please provide your IOC so that I can check your configuration and the generated the code.

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.