Skip to main content
Associate
November 12, 2025
Solved

NUCLEO-U575ZI-Q - Can't run any program using OpenOCD

  • November 12, 2025
  • 5 replies
  • 528 views

I've been beating my head for a while trying to use OpenOCD to download my program to the chip, and I'm getting error messages which cite a write algorithm error (errors attached below). I'm not really too sure what I'm doing wrong, and would greatly appreciate any help and insight with resolving this!

TL;DR. I'm getting errors like

Error: flash write algorithm aborted by target
Error: error executing stm32l4 flash write algorithm
Error: flash write failed = 00000088
Error: block write failed
Error: error writing to flash at address 0x08000000 at offset 0x00000000

in the Console log from OpenOCD.

I've reproduced the error using OpenOCD with STM32CubeIDE as follows where I set up a fresh project, demonstrate that using ST-LINK (ST-LINK GDB SERVER) works, and finally demonstrate that using OpenOCD fails.

I create a new project with

File > New > STM32 Project

And go to "Board Selector", then select the "Commercial Part Number" to NUCLEO-U575ZI-Q.

I press "Next >", then fill out the following settings and press "Finish"

lindt_1-1762964740315.png

Not sure why the following menu popped up, but I filled it out as follows and pressed "Ok"

lindt_2-1762964808489.png

Then, when I switch to the project and press

lindt_3-1762964893044.png

And press "Ok" in the following menu

lindt_4-1762964919298.png

In the console logs,

STMicroelectronics ST-LINK GDB server. Version 7.11.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.

Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.20.0 
 -------------------------------------------------------------------



Log output file: C:\Users\me\AppData\Local\Temp\STM32CubeProgrammer_a03444.log
ST-LINK SN : 0037003F3234511133353533
ST-LINK FW : V3J16M7
Board : NUCLEO-U575ZI-Q
Voltage : 3.30V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x482
Revision ID : Rev W
Device name : STM32U575/STM32U585
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0x93
Debug in Low Power mode enabled

 -------------------------------------------------------------------
 Choose flashing speed for Cortex M33 series.(default speed=Reliable) 
 -------------------------------------------------------------------



Opening and parsing file: ST-LINK_GDB_server_a03444.srec


Memory Programming ...
 File : ST-LINK_GDB_server_a03444.srec
 Size : 27.47 KB 
 Address : 0x08000000


Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 3]
Download in Progress:


File download complete
Time elapsed during download operation: 00:00:00.362



Verifying...




Time elapsed during verifying operation: 00:00:00.085


Download verified successfully 


Shutting down...
Exit.

It looks like it downloads the application successfully.

However, if I go to

Run>Debug Configurations...

Then, click the "Debugger" and change the "Debug probe" to "ST-LINK (OpenOCD)" as follows

lindt_5-1762965135751.png

 

and press "Apply" then "Close"; and finally press

lindt_6-1762965165572.png

I get the following error menu

lindt_7-1762965270448.png

And the "Console" shows

Open On-Chip Debugger 0.12.0+dev-00623-g0ba753ca7 (2025-04-30-14:17) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
clock_config
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J16M7 (API v3) VID:PID 0483:374E
Info : Target voltage: 3.299801
Info : clock speed 8000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x0be12477
Info : [STM32U575ZITxQ.ap0] Examination succeed
Info : [STM32U575ZITxQ.cpu] Cortex-M33 r0p4 processor detected
Info : [STM32U575ZITxQ.cpu] target has 8 breakpoints, 4 watchpoints
Info : [STM32U575ZITxQ.cpu] Examination succeed
Info : gdb port disabled
Info : starting gdb server for STM32U575ZITxQ.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : [STM32U575ZITxQ.cpu] external reset detected
Info : accepting 'gdb' connection on tcp/3333
CPU in Non-Secure state
[STM32U575ZITxQ.cpu] halted due to breakpoint, current mode: Thread 
xPSR: 0xf9000000 pc: 0x08000b90 msp: 0x200c0000
STM32U575ZITxQ.cpu TrustZone disabled
STM32U575ZITxQ.cpu work-area address is set to 0x20000000
Info : device idcode = 0x30016482 (STM32U57/U58xx - Rev 'unknown' : 0x3001)
Info : TZEN = 0 : TrustZone disabled by option bytes
Info : RDP level 0 (0xAA)
Info : flash size = 2048 KiB
Info : flash mode : dual-bank
Info : device idcode = 0x30016482 (STM32U57/U58xx - Rev 'unknown' : 0x3001)
Info : TZEN = 0 : TrustZone disabled by option bytes
Info : RDP level 0 (0xAA)
Info : flash size = 2048 KiB
Info : flash mode : dual-bank
Info : device idcode = 0x30016482 (STM32U57/U58xx - Rev 'unknown' : 0x3001)
Info : TZEN = 0 : TrustZone disabled by option bytes
Info : RDP level 0 (0xAA)
Info : OTP size is 512 bytes, base address is 0x0bfa0000
Info : New GDB Connection: 1, Target STM32U575ZITxQ.cpu, state: halted
Info : accepting 'gdb' connection on tcp/3333
Info : New GDB Connection: 2, Target STM32U575ZITxQ.cpu, state: halted
[STM32U575ZITxQ.cpu] halted due to breakpoint, current mode: Thread 
xPSR: 0xf9000000 pc: 0x08000b90 msp: 0x200c0000
Info : Padding image section 0 at 0x08006d4b with 1 bytes
Error: flash write algorithm aborted by target
Error: error executing stm32l4 flash write algorithm
Error: flash write failed = 00000088
Error: block write failed
Error: error writing to flash at address 0x08000000 at offset 0x00000000
[STM32U575ZITxQ.cpu] halted due to breakpoint, current mode: Thread 
xPSR: 0xf9000000 pc: 0x08000b90 msp: 0x200c0000
Info : dropped 'gdb' connection
shutdown command invoked
Info : dropped 'gdb' connection

 

So, it looks like using the Debug probe as ST-LINK (ST-LINK GDB SERVER) works (I believe this shows my hardware connection is fine), but using ST-LINK (OpenOCD) doesn't work.

I'm running STM32CubeIDE version 1.19.0 ( Help > About STM32CubeIDE)

lindt_0-1762965975527.png

 

And if it's of any help, it looks like the OpenOCD command STM32CubeIDE is running is 

C:\ST\STM32CubeIDE_1.18.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.openocd.win32_2.4.200.202505051030\tools\bin\openocd.exe "-f" "what-am-i-doing-wrong.cfg" "-s" "C:/Users/me/STM32CubeIDE/workspace_1.18.1/what-am-i-doing-wrong" "-s" "C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.3.100.202501240831/resources/openocd/st_scripts" "-s" "C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mpu.debug.openocd_2.2.1.202505211639/resources/openocd/st_scripts" "-c" "gdb_report_data_abort enable" "-c" "gdb_port 3333" "-c" "tcl_port 6666" "-c" "telnet_port 4444"

 

What am I missing / what am I doing wrong?

 

Thanks in advance for all the help :).

Best answer by Mahmoud Ben Romdhane

Hello @lindt ,

 

I reproduced your request, and the Debug of the project is finished successfully with ST-LINK (ST-LINK GDB SERVER) and with ST-LINK (OpenOCD).

I suggest that you erase the Full chip with CubeProgrammer and then run the Debug.

I will be waiting for your feedback.

 

Best Regards.

Mahmoud

 

5 replies

ST Technical Moderator
November 13, 2025

Hello @lindt 

 

Let me thank you for posting.

I am currently checking this behavior, and I will get back to you ASAP.

 

Thanks

Mahmoud 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
lindtAuthor
Associate
November 19, 2025

Hey Mahmoud,

Really appreciate the reply :). Just wanted to follow up with you -- have we managed to reproduce the issue?

Thanks!

ST Technical Moderator
November 21, 2025

Hello @lindt ,

 

I reproduced your request, and the Debug of the project is finished successfully with ST-LINK (ST-LINK GDB SERVER) and with ST-LINK (OpenOCD).

I suggest that you erase the Full chip with CubeProgrammer and then run the Debug.

I will be waiting for your feedback.

 

Best Regards.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.