Skip to main content
Associate
Dec 9, 2024 4:53 PM UTC
Solved

NUCLEO-U083RC SWV issue

Hi,
I got an issue where I can no longer activate SWV Viewer option inside debug configuration for my NUCLEO-U083RC board. The SWV checkbox is greyed out. 
Whether I create a new project or load an existing one, the SWV option is greyed out and can no longer be selected. 

Anyone got an idea what is going on?
Also I had some issues with ITM_SendChar as it would not compile. 

Debug Trace Asynchronous Sw is active. On Nucleo board I assume SWO is connected. 

Cube IDE 1.17.0.
STM32U0 V1.2 package. 

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Dec 9, 2024 5:11 PM UTC

Hello @chris84 ,

 SWV is not available for the Cortex-M0, that is why the button to enable SWV option is greyed out.

Try to use Live Expressions if you want to check a specific variable for example.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Dec 9, 2024 5:11 PM UTC

Hello @chris84 ,

 SWV is not available for the Cortex-M0, that is why the button to enable SWV option is greyed out.

Try to use Live Expressions if you want to check a specific variable for example.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
chris84Author
Associate
Dec 9, 2024 5:24 PM UTC

Hi @Imen.D 
thank you very much for quickly shed light on it. 

The fact that in Cube MX under Debug I still can activate SWO as Trace Asynchronous Sw was misleading for me.

Thanks you. Chris