Skip to main content
Muneeswaran Manokaran
Associate II
December 5, 2020
Question

Nucleo STM32H7 - Any Example available for lwIP (Ethernet PHY) without FreeRTOS

Hi,

I am new to one for Ethernet peripherals. I need to create Project in lwIP Ethernet without FreeRTOS. Already i download example Application of LwIP_HTTP_Server_Netconn_RTOS in my board successfully.But don't understand FreeRTOS concept , because of i am new to FreeRTOS concept. Any Example lwIP without FreeRTOS Implementation available. if Available means, provide the link and suggestion to make my project ASAP.

This topic has been closed for replies.

2 replies

Cartu38 OpenDev
Graduate II
December 5, 2020

Maybe not same board you're relying on but not too far about look at STM32Cube_FW_H7_V1.8.0\Projects\NUCLEO-H723ZG\Applications\LwIP

Piranha
Principal III
December 5, 2020

If one cannot grasp the RTOS concepts, then one is a beginner. But Ethernet and USB are complex and definitely not for beginners. The H7 with Cortex-M7 also is one of the most complex MCUs out there. And the worst part of the story is the fact that ST's HAL/Cube team are also incompetent beginners and haven't been able of grasping multithreading, Ethernet and everything non-trivial since the beginning of STM32 back in a year 2007.

https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet

https://community.st.com/s/question/0D50X0000BOtfhnSQB/how-to-make-ethernet-and-lwip-working-on-stm32