Solved
NUCLEO-L452 STLink debugging external MCU using SWO
- 2 replies
- 367 views
What could be the reason that configuring in CubeIDE SWV as enabled the MCU on debug flashes and stops responding? Flashing works fine both ways, SWO is connected.
Time elapsed during verifying operation: 00:00:00.082
Download verified successfully
Target is not responding, retrying...
Shutting down...
Failed to read registers from target
Error: Failed to set breakpoint at address: 0x80005c0.
Error: Failed to set more breakpoints
Failed to read all registers from target
External target MCU is STM32L412. STLink is upgraded to the latest version.
Since flashing works, SWD is connected properly.
MCU is configured as trace asynchronous Sw and there are no reconfiguration of SWD pins.