Skip to main content
YVaid.1
Visitor II
Jun 4, 2021 5:49 AM UTC
Question

Nucleo-G0B1RE Reset problem !!!!

I have recently bought Nucleo-G0B1RE Development board, When I power on, It worked perfectly I tested some programs on it and it worked very well. Then I ported my project on which I am working it executed sucessfully. But now I am facing weird problem, When I power on the nucleo board my none of the program is working !! In my project there is Monochrome graphics display used which is showing me the garbage, Even if I load the program from STM32Cube-IDE still it is not working and showing garbage on LCD. I doubt there is some reset problem on board. Please help me !!!

Thanks in advance  

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
Jun 15, 2021 11:45 AM UTC

Hi @YVaid.1​ ,

Try to make sure that the flash is erased using STM32CubeProgrammer then download your code again. Does it work this way?

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.