Skip to main content
Visitor II
Aug 19, 2025 9:50 AM UTC
Question

Nucleo-G071RB , TARGET NOT RESPONDING

stm 32 nucleo -G071RB , TARGET NOT RESPONDING

I am not able to run after dumping the code once i use the run commond after dumping i am getting 

arget is not responding, retrying...

Target is not responding, retrying...

Shutting down...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

I tried changing the USB,Workspace,and opened new project still having same issue.

I am using STM32 Cube ide version 1.12.0 and this issue same in the other latest version 1.19.0 and firmware package is STM32Cube FW_GO V1.6.2

This topic has been closed for replies.

1 reply

Ghofrane GSOURI
ST Technical Moderator
Aug 19, 2025 10:15 AM UTC

Hello @divzz 

If you are unable to connect to your STM32 Nucleo-G071RB board, try using the "Under Reset" option in STM32CubeProgrammer by selecting it in the reset mode dropdown before connecting. This approach can help establish communication with an unresponsive device. If the issue persists, test the board on another computer to rule out PC-specific issues, and consider the possibility of hardware faults with the Nucleo board.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.