Skip to main content
Associate
Aug 2, 2025 5:53 PM UTC
Question

Not getting interrupt on PC13 pin stm32h723zgt6 user button

NUCLEO-H723ZG (MB1364)

Please verify the code and check ?

 

/*
 * 001led_toggle.c
 *
 * Created on: Jul 31, 2025
 * Author: relfo
 */
#include<string.h>
#include "stm32h7xx.h"
#include "stm32h7xx_gpio_driver.h"
void delay(void)
{
	for(uint32_t i=0;i<500000;i++);
}

int main(void)
{
	GPIO_Handle_t	gpioled,ledbutton;
	memset(&gpioled,0,sizeof(gpioled));
	memset(&ledbutton,0,sizeof(ledbutton));

	gpioled.pGPIOx=GPIOB;
	gpioled.GPIO_PinConfig.GPIO_PinNumber= GPIO_PIN_NO_14;
	gpioled.GPIO_PinConfig.GPIO_PinMode=GPIO_MODE_OUTPUT;
	gpioled.GPIO_PinConfig.GPIO_PinSpeed=GPIO_SPEED_FAST;
	gpioled.GPIO_PinConfig.GPIO_PinOPType=GPIO_OP_TYPE_PP;
	gpioled.GPIO_PinConfig.GPIO_PinPuPd_control=GPIO_NO_PUPD;

	ledbutton.pGPIOx=GPIOC;
	ledbutton.GPIO_PinConfig.GPIO_PinNumber= GPIO_PIN_NO_13;
	ledbutton.GPIO_PinConfig.GPIO_PinMode=GPIO_MODE_IT_RT;
	ledbutton.GPIO_PinConfig.GPIO_PinSpeed=GPIO_SPEED_FAST;
	ledbutton.GPIO_PinConfig.GPIO_PinPuPd_control=GPIO_NO_PUPD;

	GPIO_Periclockcontrol(GPIOB, ENABLE);
	GPIO_Periclockcontrol(GPIOC, ENABLE);
	GPIO_Init(&gpioled);
	GPIO_Init(&ledbutton);

	GPIO_WriteToOutputPin(GPIOB,GPIO_PIN_NO_14,GPIO_PIN_RESET);
	GPIO_IRQPriorityConfig(IRQ_NO_EXTI15_10,5);
	GPIO_IRQInterruptConfig(IRQ_NO_EXTI15_10,ENABLE);

	while(1);

}
void EXTI15_10_IRQHandler(void)
{
//	delay();
	GPIO_IRQHandling(GPIO_PIN_NO_13);
	GPIO_ToggleOutputPin(GPIOB, GPIO_PIN_NO_14);
}
/*
 * stm32h7xx.h
 *
 * Created on: Jul 20, 2025
 * Author: relfo
 */
#include <stdint.h>
#ifndef INC_STM32H7XX_H_
#define INC_STM32H7XX_H_
#define __vo volatile
/**********************************START:Processor Specific Details **********************************/
/*
 * ARM Cortex Mx Processor NVIC ISERx register Addresses
 */

#define NVIC_ISER0 ( (__vo uint32_t*)0xE000E100 )
#define NVIC_ISER1 ( (__vo uint32_t*)0xE000E104 )
#define NVIC_ISER2 ( (__vo uint32_t*)0xE000E108 )
#define NVIC_ISER3 ( (__vo uint32_t*)0xE000E10C )


/*
 * ARM Cortex Mx Processor NVIC ICERx register Addresses
 */
#define NVIC_ICER0 			((__vo uint32_t*)0XE000E180)
#define NVIC_ICER1			((__vo uint32_t*)0XE000E184)
#define NVIC_ICER2 		((__vo uint32_t*)0XE000E188)
#define NVIC_ICER3			((__vo uint32_t*)0XE000E18C)
/*
 * ARM Cortex Mx Processor Priority Register Address Calculation
 */
#define NVIC_PR_BASE_ADDR 	((__vo uint32_t*)0xE000E400)

/*
 * ARM Cortex Mx Processor number of priority bits implemented in Priority Register
 */
#define NO_PR_BITS_IMPLEMENTED 4
/*
 * base addresses of FLASH and SRAM
 */
#define FLASH_BASEADDR 0x08000000U // FLASH MEMORY BASE ADDRESS
#define SRAM1_BASEADDR 0x30000000U
#define SRAM2_BASEADDR 0x30004000U
#define ROM_BASEADDR	0x1FF00000U //SYSTEM MEMORY
#define SRAM SRAM1_BASEADDR
/*
 * AHBx and APBx Bus Peripheral base address
 */
#define PERIPH_BASE	 0x40000000U
#define APB1PERIPH_BASE	0x40000000U
#define APB2PERIPH_BASE	0x40010000U
#define APB3PERIPH_BASE 0x50000000U
#define APB4PERIPH_BASE	0x58000000U
#define AHB1PERIPH_BASE 0x40020000U
#define AHB2PERIPH_BASE	0x48020000U
#define AHB3PERIPH_BASE	0x51000000U
#define AHB4PERIPH_BASE	0x58020000U
/*
 * BASE ADDRESS OF PERIPHERAL HANGING ON THE AHB4 BUS
 */
#define GPIOA_BASEADDR	(AHB4PERIPH_BASE + 0x0000)
#define GPIOB_BASEADDR	(AHB4PERIPH_BASE + 0x0400)
#define GPIOC_BASEADDR	(AHB4PERIPH_BASE + 0x0800)
#define GPIOD_BASEADDR	(AHB4PERIPH_BASE + 0x0C00)
#define GPIOE_BASEADDR	(AHB4PERIPH_BASE + 0x1000)
#define GPIOF_BASEADDR	(AHB4PERIPH_BASE + 0x1400)
#define GPIOG_BASEADDR	(AHB4PERIPH_BASE + 0x1800)
#define GPIOH_BASEADDR	(AHB4PERIPH_BASE + 0x1C00)
#define GPIOJ_BASEADDR	(AHB4PERIPH_BASE + 0x2400)
#define GPIOK_BASEADDR	(AHB4PERIPH_BASE + 0x2800)
#define RCC_BASEADDR	(AHB4PERIPH_BASE + 0x4400)
/*
 * BASE ADDRESS OF THE PERIPHERAL HANGING ON APB1 BUS
 */
#define I2C1_BASEADDR (APB1PERIPH_BASE + 0x5400)
#define I2C2_BASEADDR (APB1PERIPH_BASE + 0x5800)
#define I2C3_BASEADDR (APB1PERIPH_BASE + 0x5C00)
#define I2C5_BASEADDR (APB1PERIPH_BASE + 0x6400)
#define SPI2_BASEADDR (APB1PERIPH_BASE + 0x3800)
#define USART2_BASEADDR	(APB1PERIPH_BASE +	0x4400)
#define UART4_BASEADDR	(APB1PERIPH_BASE +	0x4C00)
/*
 * BASE ADDRESS OF THE PERIPHERAL HANGING ON APB2BUS
 */
/*
 * BASE ADDRESS OF THE PERIPHERAL HANGING ON APB3 BUS
 */
/*
 * BASE ADDRESS OF THE PERIPHERAL HANGING ON APB4 BUS
 */
#define EXTI_BASEADDR	(APB4PERIPH_BASE + 0x0000)
#define SYSCFG_BASEADDR (APB4PERIPH_BASE + 0x0400)

/*******************************PERIPERAL REGISTER DEFINATION STRUCTURE FOR GPIO *****************/
typedef struct
{
	__vo uint32_t MODER; // GPIO port mode register 				 ADDRESS OFFSET 0x0000
	__vo uint32_t OTYPER; // GPIO port output type register
	__vo uint32_t OSPEEDR; // GPIO port output speed register
	__vo uint32_t PUPDR; // GPIO port pull-up/pull-down register
	__vo uint32_t IDR;
	__vo uint32_t ODR;
	__vo uint32_t BSRR;
	__vo uint32_t LCKR;
	__vo uint32_t AFR[2];

}GPIO_RegDef_t;
/*
 * *****************************RCC REGISTER DEFINATION STRUCTURE*******************************
 */
typedef struct
{
	__vo uint32_t CR;		 //address offset 0x000
	__vo uint32_t HSICFGR; //address offset 0x004
	__vo uint32_t CRRCR;	 //address offset 0x008
	__vo uint32_t CSICFGR;	 //address offset 0x00C
	__vo uint32_t CFGR;		 //address offset 0x010
	 uint32_t reserved1; //address offset 0x014
	__vo uint32_t D1CFGR;	 //address offset 0x018
	__vo uint32_t D2CFGR;	 //address offset 0x01C
	__vo uint32_t D3CFGR;	 //address offset 0x020
		 uint32_t reserved2; //address offset 0x024
	__vo uint32_t PLLCKSELR; //address offset 0x028
	__vo uint32_t PLLCFGR;	 //address offset 0x02C
	__vo uint32_t PLL1DIVR;	 //address offset 0x030
	__vo uint32_t PLL1FRACR; //address offset 0x034
	__vo uint32_t PLL2DIVR;	 //address offset 0x038
	__vo uint32_t PLL2FRACR; //address offset 0x03C
	__vo uint32_t PLL3DIVR;	 //address offset 0x040
	__vo uint32_t PLL3FRACR; //address offset 0x044
		 uint32_t reserved3; //address offset 0x048
	__vo uint32_t D1CCIPR;	 //address offset 0x04C
	__vo uint32_t D2CCIP1R;	 //address offset 0x050
	__vo uint32_t D2CCIP2R;	 //address offset 0x054
	__vo uint32_t D3CCIPR;	 //address offset 0x058
	 uint32_t reserved4; //address offset 0x05C
	__vo uint32_t CIER;	 //address offset 0x060
	__vo uint32_t CIFR;	 //address offset 0x064
	__vo uint32_t CICR;	 //address offset 0x068
	 uint32_t reserved5; //address offset 0x06C
	__vo uint32_t BDCR;	 //address offset 0x070
	__vo uint32_t CSR;	 //address offset 0x074
	 uint32_t reserved6; //address offset 0x078
	__vo uint32_t AHB3RSTR;	 //address offset 0x07C
	__vo uint32_t AHB1RSTR;	 //address offset 0x080
	__vo uint32_t AHB2RSTR;	 //address offset 0x084
	__vo uint32_t AHB4RSTR;	 //address offset 0x088
	__vo uint32_t APB3RSTR;	 //address offset 0x08C
	__vo uint32_t APB1LRSTR; //address offset 0x090
	__vo uint32_t APB1HRSTR; //address offset 0x094
	__vo uint32_t APB2RSTR; //address offset 0x098
	__vo uint32_t APB4RSTR; //address offset 0x09C
	__vo uint32_t GCR; //address offset 0x0A0
 uint32_t reserved7; //address offset 0x0A4
	__vo uint32_t D3AMR; //address offset 0x0A8
	 uint32_t reserved8[9];//address offset0x0AC-0x0CC
	__vo uint32_t RSR; //address offset 0x0D0
	__vo uint32_t AHB3ENR; //address offset 0x0D4
	__vo uint32_t AHB1ENR; //address offset 0x0D8
	__vo uint32_t AHB2ENR; //address offset 0x0DC
	__vo uint32_t AHB4ENR; //address offset 0x0E0
	__vo uint32_t APB3ENR; //address offset 0x0E4
	__vo uint32_t APB1LENR; //address offset 0x0E8
	__vo uint32_t APB1HENR; //address offset 0x0EC
	__vo uint32_t APB2ENR; //address offset 0x0F0
	__vo uint32_t APB4ENR; //address offset 0x0F4
	 uint32_t reserved9; //address offset 0x0F8
	__vo uint32_t AHB3LPENR; //address offset 0x0FC
	__vo uint32_t AHB1LPENR; //address offset 0x100
	__vo uint32_t AHB2LPENR; //address offset 0x104
	__vo uint32_t AHB4LPENR; //address offset 0x108
	__vo uint32_t APB3LPENR; //address offset 0x10C
	__vo uint32_t APB1LLPENR; //address offset 0x110
	__vo uint32_t APB1HLPENR; //address offset 0x114
	__vo uint32_t APB2LPENR; //address offset 0x118
	__vo uint32_t APB4LPENR; //address offset 0x11C
	 uint32_t reserved10[4]; //address offset 0x120-0x12C
	__vo uint32_t C1_RSR; //address offset 0x130
	__vo uint32_t C1_AHB3ENR; //address offset 0x134
	__vo uint32_t C1_AHB1ENR; //address offset 0x138
	__vo uint32_t C1_AHB2ENR; //address offset 0x13C
	__vo uint32_t C1_AHB4ENR; //address offset 0x140
	__vo uint32_t C1_APB3ENR; //address offset 0x144
	__vo uint32_t C1_APB1LENR;//address offset 0x148
	__vo uint32_t C1_APB1HENR;//address offset 0x14C
	__vo uint32_t C1_APB2ENR; //address offset 0x150
	__vo uint32_t C1_APB4ENR; //address offset 0x154
	 uint32_t reserved11; //address offset 0x158
	__vo uint32_t C1_AHB3LPENR;//address offset 0x15C
	__vo uint32_t C1_AHB1LPENR;//address offset 0x160
	__vo uint32_t C1_AHB2LPENR;//address offset 0x164
	__vo uint32_t C1_AHB4LPENR;//address offset 0x168
	__vo uint32_t C1_APB3LPENR;//address offset 0x16C
	__vo uint32_t C1_APB1LLPENR;//address offset 0x170
	__vo uint32_t C1_APB1HLPENR;//address offset 0x174
	__vo uint32_t C1_APB2LPENR;//address offset 0x178
	__vo uint32_t C1_APB4LPENR;//address offset 0x17C
	 uint32_t reserved12[32];//address offset 0x180-0x1FC

}RCC_RegDef_t;
/*******************************PERIPERAL REGISTER DEFINATION STRUCTURE FOR EXTI *****************/
typedef struct
{
	__vo uint32_t	RTSR1;			//address offset 0x00
	__vo uint32_t	FTSR1;			//address offset 0x04
	__vo uint32_t	SWIER1;			//address offset 0x08
	__vo uint32_t	D3PMR1;			//address offset 0x0C
	__vo uint32_t	D3PCR1L;		//address offset 0x10
	__vo uint32_t	D3PCR1H;		//address offset 0x14
	__vo uint32_t	RTSR2;			//address offset 0x20
	__vo uint32_t	FTSR2;			//address offset 0x24
	__vo uint32_t	SWIER2;			//address offset 0x28
	__vo uint32_t	D3PMR2;			//address offset 0x2C
	__vo uint32_t	D3PCR2L;		//address offset 0x30
	__vo uint32_t	D3PCR2H;		//address offset 0x34
	__vo uint32_t	RTSR3;			//address offset 0x40
	__vo uint32_t	FTSR3;			//address offset 0x44
	__vo uint32_t	SWIER3;			//address offset 0x48
	__vo uint32_t	D3PMR3;			//address offset 0x4C
	__vo uint32_t	D3PCR3L;		//address offset 0x50
	__vo uint32_t	D3PCR3H;		//address offset 0x54
	 uint32_t	reserved1[10]; //address offset 0x58-0x7C
	__vo uint32_t	CPUIMR1;		//address offset 0x80
	__vo uint32_t	CPUEMR1;		//address offset 0x84
	__vo uint32_t	CPUPR1;			//address offset 0x88
	__vo uint32_t	CPUIMR2;		//address offset 0x90
	__vo uint32_t	CPUEMR2;		//address offset 0x94
	__vo uint32_t	CPUPR2;			//address offset 0x98
	__vo uint32_t	CPUIMR3;		//address offset 0xA0
	__vo uint32_t	CPUEMR3;		//address offset 0xA4
	__vo uint32_t	CPUPR3;			//address offset 0xA8
		 uint32_t	reserved2[5];	//address offset 0xAC-0xBC

}EXTI_RegDef_t;
/*******************************PERIPERAL REGISTER DEFINATION STRUCTURE FOR SYSCFG *****************/
typedef struct
{
	__vo uint32_t reserved1; //address offset 0x00
	__vo uint32_t	PMCR;		 //address offset 0x04
	__vo uint32_t	EXTICR[4]; //address offset 0x08-0x14
	__vo uint32_t	CFGR;		 //address offset 0x18
	__vo uint32_t	reserved2; //address offset 0x1C
	__vo uint32_t CCCSR;		//address offset 0x20
	__vo uint32_t CCVR; //address offset 0x24
	__vo uint32_t 	CCCR;		 //address offset 0x28
	__vo uint32_t	reserved3;	 //address offset 0x2C
	__vo uint32_t	ADC2ALT;	 //address offset 0x30
	__vo uint32_t reserved4[60];//address offset 0x34 to 0x120
	__vo uint32_t 	PKGR;		 //address offset 0x124
	__vo uint32_t	reserved5[118];//address offset 0x128- 0x2FC
	__vo uint32_t	UR0;		 //address offset 0x300
	__vo uint32_t	reserved6; //address offset 0x304
 __vo uint32_t	UR2;
 __vo uint32_t	UR3;
 __vo uint32_t	UR4;
 __vo uint32_t	UR5;
 __vo uint32_t	UR6;
 __vo uint32_t	UR7;
 __vo uint32_t	reserved7[3];
 __vo uint32_t	UR11;
 __vo uint32_t	UR12;
 __vo uint32_t	UR13;
 __vo uint32_t	UR14;
 __vo uint32_t	UR15;
 __vo uint32_t	UR16;
 __vo uint32_t	UR17;
 
}SYSCFG_RegDef_t;
/*
 * PERIPHERAL DEFINATION (PERIPHERAL BASE ADDRESS TYPECASTED TO REGDEF)
 */
#define GPIOA	((GPIO_RegDef_t*)GPIOA_BASEADDR)
#define GPIOB	((GPIO_RegDef_t*)GPIOB_BASEADDR)
#define GPIOC	((GPIO_RegDef_t*)GPIOC_BASEADDR)
#define GPIOD	((GPIO_RegDef_t*)GPIOD_BASEADDR)
#define GPIOE	((GPIO_RegDef_t*)GPIOE_BASEADDR)
#define GPIOF	((GPIO_RegDef_t*)GPIOF_BASEADDR)
#define GPIOG	((GPIO_RegDef_t*)GPIOG_BASEADDR)
#define GPIOH	((GPIO_RegDef_t*)GPIOH_BASEADDR)
#define GPIOJ	((GPIO_RegDef_t*)GPIOJ_BASEADDR)
#define GPIOK	((GPIO_RegDef_t*)GPIOK_BASEADDR)

#define RCC	 ((RCC_RegDef_t*)RCC_BASEADDR)
#define EXTI	((EXTI_RegDef_t*)EXTI_BASEADDR)
#define SYSCFG	((SYSCFG_RegDef_t*)SYSCFG_BASEADDR)
/*
 * CLOCK ENABLE MACRO FOR GPIOx PERIPHERAL
 */
#define GPIOA_PCLK_EN() (RCC->AHB4ENR |= (1<<0))
#define GPIOB_PCLK_EN()		(RCC->AHB4ENR |= (1<<1))
#define GPIOC_PCLK_EN()		(RCC->AHB4ENR |= (1<<2))
#define GPIOD_PCLK_EN()		(RCC->AHB4ENR |= (1<<3))
#define GPIOE_PCLK_EN()		(RCC->AHB4ENR |= (1<<4))
#define GPIOF_PCLK_EN()		(RCC->AHB4ENR |= (1<<5))
#define GPIOG_PCLK_EN()		(RCC->AHB4ENR |= (1<<6))
#define GPIOH_PCLK_EN()		(RCC->AHB4ENR |= (1<<7))
#define GPIOJ_PCLK_EN()		(RCC->AHB4ENR |= (1<<9))
#define GPIOK_PCLK_EN()		(RCC->AHB4ENR |= (1<<10))

/*
 * CLOCK ENABLE MACRO FOR I2Cx PERIPHERAL
 */
#define I2C1_PCLK_EN() (RCC->APB1LENR |= (1<<21))
#define I2C2_PCLK_EN()	(RCC->APB1LENR |= (1<<22))
#define I2C3_PCLK_EN()	(RCC->APB1LENR |= (1<<23))
#define I2C5_PCLK_EN()	(RCC->APB1LENR |= (1<<25))
/*
 * CLOCK ENABLE MACRO FOR SPIx PERIPHERAL
 */
#define SPI2_PCLK_EN()		(RCC->APB1LENR |= (1<<14))
/*
 * CLOCK ENABLE MACRO FOR USARTx PERIPHERAL
 */
#define USART2_PCLK_EN()	(RCC->APB1LENR |= (1<<17))
/*
 * CLOCK ENABLE MACRO FOR UARTx PERIPHERAL
 */
#define UART4_PCLK_EN()		(RCC->APB1LENR |= (1<<19))
/*
 * CLOCK ENABLE MACRO FOR SYSCONFIG PERIPHERAL
 */
#define	SYSCFG_PCLK_EN()	(RCC->APB4ENR |= (1<<1))
/*
 * CLOCK DISABLE MACRO FOR GPIOx PERIPHERAL
 */
#define GPIOA_PCLK_DI() (RCC->AHB4ENR &=~(1<<0))
#define GPIOB_PCLK_DI()		(RCC->AHB4ENR &=~(1<<1))
#define GPIOC_PCLK_DI()		(RCC->AHB4ENR &=~(1<<2))
#define GPIOD_PCLK_DI()		(RCC->AHB4ENR &=~(1<<3))
#define GPIOE_PCLK_DI()		(RCC->AHB4ENR &=~(1<<4))
#define GPIOF_PCLK_DI()		(RCC->AHB4ENR &=~(1<<5))
#define GPIOG_PCLK_DI()		(RCC->AHB4ENR &=~(1<<6))
#define GPIOH_PCLK_DI()		(RCC->AHB4ENR &=~(1<<7))
#define GPIOJ_PCLK_DI()		(RCC->AHB4ENR &=~(1<<9))
#define GPIOK_PCLK_DI()		(RCC->AHB4ENR &=~(1<<10))

/*
 * CLOCK DISABLE MACRO FOR I2Cx PERIPHERAL
 */
#define I2C1_PCLK_DI() (RCC->APB1LENR &=~(1<<21))
#define I2C2_PCLK_DI()	(RCC->APB1LENR &=~(1<<22))
#define I2C3_PCLK_DI()	(RCC->APB1LENR &=~(1<<23))
#define I2C5_PCLK_DI()	(RCC->APB1LENR &=~(1<<25))
/*
 * CLOCK DISABLE MACRO FOR SPIx PERIPHERAL
 */
#define SPI2_PCLK_DI()	(RCC->APB1LENR &=~(1<<14))
/*
 * CLOCK DISABLE MACRO FOR USARTx PERIPHERAL
 */
#define USART2_PCLK_DI()	(RCC->APB1LENR &=~(1<<17))
/*
 * CLOCK DISABLE MACRO FOR UARTx PERIPHERAL
 */
#define UART4_PCLK_DI()		(RCC->APB1LENR &=~(1<<19))
/*
 * MACROS TO RESET THE GPIOx PERIPHERALS
 */
#define GPIOA_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<0)) ; (RCC->AHB4RSTR &=~(1<<0));}while(0)
#define GPIOB_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<1)) ; (RCC->AHB4RSTR &=~(1<<1));}while(0)
#define GPIOC_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<2)) ; (RCC->AHB4RSTR &=~(1<<2));}while(0)
#define GPIOD_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<3)) ; (RCC->AHB4RSTR &=~(1<<3));}while(0)
#define GPIOE_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<4)) ; (RCC->AHB4RSTR &=~(1<<4));}while(0)
#define GPIOF_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<5)) ; (RCC->AHB4RSTR &=~(1<<5));}while(0)
#define GPIOG_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<6)) ; (RCC->AHB4RSTR &=~(1<<6));}while(0)
#define GPIOH_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<7)) ; (RCC->AHB4RSTR &=~(1<<7));}while(0)
#define GPIOJ_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<9)) ; (RCC->AHB4RSTR &=~(1<<9));}while(0)
#define GPIOK_REG_RESET()	do{(RCC->AHB4RSTR |=(1<<10)); (RCC->AHB4RSTR &=~(1<<10));}while(0)
/*
 * MACRO FOR GPIO BASEADDR TO CODE
 */
#define GPIO_BASEADDR_TO_CODE(X)	 ((X==GPIOA)?0:\
								 	 (X==GPIOB)?1:\
								 	 (X==GPIOC)?2:\
									 (X==GPIOD)?3:\
		 (X==GPIOE)?4:\
			 (X==GPIOF)?5:\
						 (X==GPIOG)?6:\
						 (X==GPIOH)?7:\
						 (X==GPIOJ)?8:\
						 (X==GPIOK)?9:0)
/*
 * IRQ(Interrupt Request) Numbers of STM32h7x MCU
 * NOTE: update these macros with valid values according to your MCU
 * TODO: You may complete this list for other peripherals
 */

#define IRQ_NO_EXTI0 		6
#define IRQ_NO_EXTI1 		7
#define IRQ_NO_EXTI2 		8
#define IRQ_NO_EXTI3 		9
#define IRQ_NO_EXTI4 		10
#define IRQ_NO_EXTI9_5 		23
#define IRQ_NO_EXTI15_10 	40
/*
 * macros for all the possible priority levels
 */
#define NVIC_IRQ_PRI0 0
#define NVIC_IRQ_PRI15 15
/*
 * some generic macros
 */
#define ENABLE 			1
#define DISABLE			0
#define SET				ENABLE
#define RESET 			DISABLE
#define GPIO_PIN_SET 	SET
#define GPIO_PIN_RESET 	RESET

#endif /* INC_STM32H7XX_H_ */

 

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
Aug 3, 2025 1:41 AM UTC

Check that SB51 / PC13 is bridged, and not SB58 / PA0

SB51 is on the underside, behind the button

Perhaps build an example using the HAL rather than custom library. If that works debug your library

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
prash9822Author
Associate
Aug 3, 2025 6:56 AM UTC

Using Hal it is working but I want why it is not working with my library can you check my library and review code please

waclawek.jan
Super User
Aug 3, 2025 7:54 AM UTC

Read you and check/post/compare-to-working relevant GPIO, EXTI, NVIC registers content. 

JW

prash9822Author
Associate
Aug 3, 2025 6:13 PM UTC

can you review files i tried but getting any hope

 

waclawek.jan
Super User
Aug 4, 2025 10:14 AM UTC

As I've said, if you have working and non-working code, you can find the problem yourself by comparing registers content between the working and non-working case.

JW