Skip to main content
lauris
Associate III
May 19, 2025 1:50 PM UTC
Solved

Not compiling SUBG2 generated project and not sure if working after fixing it

Hello,

I want to try out 6LowPan on S2LP and found that in SUBG2 module I can do that on Contiki. Everything is being built on `NUCLEO-H753ZI` + `NUCLEO-S2868A2`. But after trying to generate code I found few issues in order to make it compile. Maybe it is some misconfiguration, some bugs or mixture of both. But basically issues I found with their fixes I have applied are as follows:

  1. even before `SUBG2` project was missing `NUCLEO...` defines in `stm32h7xx_nucleo_conf.h` and what is frustrating is that there is no user code place so what I have added is being removed after each code generation. Solution following lines added to `stm32h7xx_nucleo_conf.h`:
#define USE_NUCLEO_144
#define USE_NUCLEO_H753ZI​
  • COM (Serial interface) initialization is generated with single argument, while Function requires 2. Solution was add `COM_InitTypeDef` variable and pass it too in `contiki-platform.c`.
- BSP_COM_Init(COM1);
+ COM_InitTypeDef comInit = {.BaudRate = 115200,
+				.WordLength = UART_WORDLENGTH_8B,
+				.Parity = UART_PARITY_NONE,
+				.StopBits = UART_STOPBITS_1,
+				.HwFlowCtl = UART_HWCONTROL_NONE};
+ BSP_COM_Init(COM1, &comInit);​
  • `SUBG2` timer callback conflicting with system timer callback. Solution was comment out Contiki timer callback function in `subg2_contiki_it.c`:
//#if (USE_HAL_TIM_REGISTER_CALLBACKS == 1)
//void SUBG2_RTIMER_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
//#else
//void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
//#endif /*USE_HAL_TIM_REGISTER_CALLBACKS*/
//{
// if(htim->Instance == SUBG2_RTIMER_INSTANCE)
// {
// __HAL_TIM_CLEAR_FLAG(&contiki_rtimer, TIM_FLAG_UPDATE);
// }
//}​

and add Contiki timer clearing in system timer callback:

 /* Private includes ----------------------------------------------------------*/
 /* USER CODE BEGIN Includes */
+#include "subg2_bsp_ip_conf.h"
 
 /* USER CODE END Includes */


...

 void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
 {
 /* USER CODE BEGIN Callback 0 */
 
 /* USER CODE END Callback 0 */
 if (htim->Instance == TIM13) {
 HAL_IncTick();
 }
 /* USER CODE BEGIN Callback 1 */
+ if(htim->Instance == SUBG2_RTIMER_INSTANCE)
+ {
+ __HAL_TIM_CLEAR_FLAG(&contiki_rtimer, TIM_FLAG_UPDATE);
+ }
 /* USER CODE END Callback 1 */
 }
  • [UDP client app only] `HAL_TIM_PERIOD_ELAPSED_CB_ID` is undefined and seems to be defined only with `USE_HAL_TIM_REGISTER_CALLBACKS` defined, but no idea how to define it from project side. As of solution just that part was commented out assuming `HAL_TIM_PeriodElapsedCallback()` will be called. Changes to `stm32h7xx_hal_timebase_tim.c`:
 /* Private function prototypes -----------------------------------------------*/
- void TimeBase_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim);
 /* Private functions ---------------------------------------------------------*/

...

 if(HAL_TIM_Base_Init(&htim13) == HAL_OK)
 {
 /* Start the TIM time Base generation in interrupt mode */
 return HAL_TIM_Base_Start_IT(&htim13);
 }
- HAL_TIM_RegisterCallback(&htim13, HAL_TIM_PERIOD_ELAPSED_CB_ID, TimeBase_TIM_PeriodElapsedCallback);
 
 /* Return function status */
 return HAL_ERROR;

...

- /**
- * @brief Period elapsed callback in non blocking mode
- * @note This function is called when TIM6 interrupt took place, inside
- * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
- * a global variable "uwTick" used as application time base.
- * @PAram htim TIM handle
- * @retval None
- */
-
-void TimeBase_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
-{
- /* Prevent unused argument(s) compilation warning */
- UNUSED(htim);
-
- HAL_IncTick();
-}​

And after all these changes I have `UDP server` and `UDP Client` apps running side by side. But not working/communicating. Or I do not know how to test them. Since I assume they should see each other and client would broadcast some message and server receive and echo it back, and I would see that in their log. But no what I see on server side is:

[INFO: S2LP_platform] Starting Contiki-NG
[INFO: S2LP_platform] - Routing: RPL Lite
[INFO: S2LP_platform] - Net: sicslowpan
[INFO: S2LP_platform] - MAC: CSMA
[INFO: S2LP_platform] - 802.15.4 PANID: 0xabcd
[INFO: S2LP_platform] - 802.15.4 Default channel: 0
[INFO: S2LP_platform] Node ID: 32050
[INFO: S2LP_platform] Link-layer address: 0e51.3332.6f33.7d32
[INFO: RPL ] initializing
[INFO: S2LP_platform] Tentative link-local IPv6 address: fe80::c51:3332:6f33:7d32
[INFO: S2LP_platform] ST S2LP Platform
Platform and Contiki-NG parameters:
"Board: stm32h7xx_nucleo":	"Board: stm32h7xx_nucleo"
"Expansion Board: S2868A2":	"Expansion Board: S2868A2"

RSSI_RX_THRESHOLD:	-118.0
RSSI_TX_THRESHOLD:	-90.0
RADIO_HW_CSMA:	1
POWER_DBM:	12.0
CHANNEL_SPACE:	100e3
FREQ_DEVIATION:	20e3
BANDWIDTH:	100.0e3
MODULATION_SELECT:	MOD_2FSK
DATARATE:	38400
IEEE802154_CONF_PANID:	abcd
BASE_FREQUENCY:	868.0e6
CHANNEL_NUMBER:	0
MAX_PACKET_LEN:	128

UIP_CONF_BUFFER_SIZE:	1280
UIP_CONF_ROUTER:	1
UIP_CONF_IPV6_RPL:	1
RPL_DEFAULT_LEAF_ONLY:	0
QUEUEBUF_CONF_NUM:	8
UIP_ND6_REACHABLE_TIME:	60000
UIP_TCP_MSS:	1220
UIP_RECEIVE_WINDOW:	1220
UIP_CONF_TCP:	0
UIP_MAX_ROUTES:	0
NBR_TABLE_CONF_MAX_NEIGHBORS:	16
UIP_CONF_ND6_SEND_RA:	0
UIP_CONF_ND6_SEND_NA:	1
UIP_CONF_ND6_SEND_NS:	0
IP64 is disabled.
DTLS is disabled.
RADIO_LOW_POWER:	0
RADIO_SNIFF_MODE:	0
RADIO_LONG_PREAMBLE:	0

[INFO: S2LP_platform] Contiki-NG and Sub-GHz Radio correctly configured... Starting all processes
[INFO: RPL ] IPv6 addresses:
[INFO: RPL ] -- fd00::c51:3332:6f33:7d32
[INFO: RPL ] -- fe80::c51:3332:6f33:7d32
[INFO: RPL ] reset DIO timer (Init root)
[INFO: RPL ] created DAG with instance ID 0, DAG ID fd00::c51:3332:6f33:7d32, rank 128
[INFO: RPL ] created a new RPL DAG
[INFO: RPL ] sending a multicast-DIO with rank 128 to ff02::1a
[INFO: CSMA ] sending to 0000.0000.0000.0000, len 80, seqno 70, queue length 1, free packets 7
[DBG : CSMA ] scheduling transmission in 24 ticks, NB=0, BE=3
[INFO: CSMA ] preparing packet for 0000.0000.0000.0000, seqno 70, tx 0, queue 1

And on client is:

[INFO: S2LP_platform] Starting Contiki-NG
[INFO: S2LP_platform] - Routing: RPL Lite
[INFO: S2LP_platform] - Net: sicslowpan
[INFO: S2LP_platform] - MAC: CSMA
[INFO: S2LP_platform] - 802.15.4 PANID: 0xabcd
[INFO: S2LP_platform] - 802.15.4 Default channel: 0
[INFO: S2LP_platform] Node ID: 23602
[INFO: S2LP_platform] Link-layer address: 0e51.3332.6133.5c32
[INFO: RPL ] initializing
[INFO: S2LP_platform] Tentative link-local IPv6 address: fe80::c51:3332:6133:5c32
[INFO: S2LP_platform] ST S2LP Platform
Platform and Contiki-NG parameters:
"Board: stm32h7xx_nucleo":	"Board: stm32h7xx_nucleo"
"Expansion Board: S2868A2":	"Expansion Board: S2868A2"

RSSI_RX_THRESHOLD:	-118.0
RSSI_TX_THRESHOLD:	-90.0
RADIO_HW_CSMA:	1
POWER_DBM:	12.0
CHANNEL_SPACE:	100e3
FREQ_DEVIATION:	20e3
BANDWIDTH:	100.0e3
MODULATION_SELECT:	MOD_2FSK
DATARATE:	38400
IEEE802154_CONF_PANID:	abcd
BASE_FREQUENCY:	868.0e6
CHANNEL_NUMBER:	0
MAX_PACKET_LEN:	128

UIP_CONF_BUFFER_SIZE:	1280
UIP_CONF_ROUTER:	1
UIP_CONF_IPV6_RPL:	1
RPL_DEFAULT_LEAF_ONLY:	0
QUEUEBUF_CONF_NUM:	8
UIP_ND6_REACHABLE_TIME:	60000
UIP_TCP_MSS:	1220
UIP_RECEIVE_WINDOW:	1220
UIP_CONF_TCP:	0
UIP_MAX_ROUTES:	0
NBR_TABLE_CONF_MAX_NEIGHBORS:	16
UIP_CONF_ND6_SEND_RA:	0
UIP_CONF_ND6_SEND_NA:	1
UIP_CONF_ND6_SEND_NS:	0
IP64 is disabled.
DTLS is disabled.
RADIO_LOW_POWER:	0
RADIO_SNIFF_MODE:	0
RADIO_LONG_PREAMBLE:	0

[INFO: S2LP_platform] Contiki-NG and Sub-GHz Radio correctly configured... Starting all processes
[INFO: App ] Not reachable yet
[INFO: App ] Not reachable yet
[INFO: App ] Not reachable yet
[INFO: App ] Not reachable yet
[INFO: RPL ] sending a DIS to ff02::1a
[INFO: CSMA ] sending to 0000.0000.0000.0000, len 10, seqno 152, queue length 1, free packets 7
[DBG : CSMA ] scheduling transmission in 29 ticks, NB=0, BE=3
[INFO: CSMA ] preparing packet for 0000.0000.0000.0000, seqno 152, tx 0, queue 1

 

Bother devices are started/restarted same time and next to each other.

So all that boils down to 3 main questions:

  1. Are there some faults in configuration in order to avoid these code changes to make code compile? If not probably is some sort of a bug in `STM32CCubeIDE`.
  2. Can my fixes be responsible for examples not working as I expect. I would expect some kind of ping/pong scenario where `UDP client` broadcast `ping` and `UDP server` after receiving it sends back `pong`.
  3. My assumption of example is wrong and should be changed somehow (code added, other app compiled, or other) in order to make some data being transmitted over `6lowpan`?

Project `*.ioc` file of `UDP client` is attached if it would be of any help.

Thank you in advance for any help.

 

@SUBG2 @6lowpan @S2LP @Contiki

This topic has been closed for replies.
Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jun 3, 2025 7:48 AM UTC

Hello @lauris 

Regarding the compilation errors :

There is a limitation regarding the compatibility of Start From Board with X-CUBE-SUBG2. This issue is documented in the Start From Board wiki.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Ghofrane GSOURI
ST Technical Moderator
May 20, 2025 8:06 AM UTC

Hello @lauris 

First let me thank you for posting .

I'm currently investigating this issue. I will get back to you as soon as possible.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ghofrane GSOURI
ST Technical Moderator
May 20, 2025 3:32 PM UTC

Hello @lauris 

I sincerely appreciate you bringing these issues to our attention.

Ticket has been raised to dev team.

Internal ticket number 210193

I will keep you posted with updates.

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
lauris
laurisAuthor
Associate III
Jun 3, 2025 7:23 AM UTC

Hello Ghofrane,

Any news regarding this issue?

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jun 3, 2025 7:48 AM UTC

Hello @lauris 

Regarding the compilation errors :

There is a limitation regarding the compatibility of Start From Board with X-CUBE-SUBG2. This issue is documented in the Start From Board wiki.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.