Skip to main content
YMaha
Associate
March 21, 2024
Question

Not able to use HAL_UARTEx_ReceiveToIdle_IT & HAL_UART_Receive simultaneously

Hello,

I am trying to use USART peripheral of my STM32F303VCT6 based board. 

I want to receive the data on serial line and size of the data is not fixed or known beforehand. Once the particular string of data is received, I compare it with predefined strings stored in various arrays & based on the match, which of the if/else codes in while loop should be implemented, is decided.

In the If/else code, I also want to receive the data from same USART but this data is not to be used for the comparison above & length of this data is known. Once If/else code is executed, program should again wait for new string for comparison.

For this, I have used HAL_UARTEx_ReceiveToIdle_IT & HAL_UART_Receive  as given in the code snippet below,

 

Callback Function is -

 

 

void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
	FS1State=memcmp((uint8_t *) globalRxBuff,FS1,sizeof(FS1));			
	FS2State=memcmp((uint8_t *) globalRxBuff,FS2,sizeof(FS2));			
	FS3State=memcmp((uint8_t *) globalRxBuff,FS3,sizeof(FS3));			
	FS4State=memcmp((uint8_t *) globalRxBuff,FS4,sizeof(FS4));	
 if(FS1State==0)
	{
	page=1;
	}
	else if(FS2State==0)
	{
	page=2;
	}
	else if(FS3State==0)
	{
	page=3;
	}
	else if(FS4State==0)
	{
	page=4;
	}	
 memset((uint8_t *) globalRxBuff,0x00,27);
	HAL_UARTEx_ReceiveToIdle_IT(&huart2, (uint8_t*)globalRxBuff, 100);
}

	

 

 

While loop -

 

while(1)
{
if(page==1)
{
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE); //Disabling the RXNE Interrupt
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE); // Disabling the Idle Line Interrupt
huart2.RxState= HAL_UART_STATE_READY;
HAL_UART_Transmit(&huart2,txBuff,10,HAL_MAX_DELAY);
HAL_UART_Receive(&huart2, page1RxBuff, 6, HAL_MAX_DELAY);
SET_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE);
SET_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE);
}
else if(page==2)
{
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE); //Disabling the RXNE Interrupt
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE); // Disabling the Idle Line Interrupt
huart2.RxState= HAL_UART_STATE_READY;
HAL_UART_Transmit(&huart2,txBuff,10,HAL_MAX_DELAY);
HAL_UART_Receive(&huart2, page2RxBuff, 6, HAL_MAX_DELAY);
SET_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE);
SET_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE);
}
else if(page==3)
{
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE); //Disabling the RXNE Interrupt
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE); // Disabling the Idle Line Interrupt
huart2.RxState= HAL_UART_STATE_READY;
HAL_UART_Transmit(&huart2,txBuff,10,HAL_MAX_DELAY);
HAL_UART_Receive(&huart2, page3RxBuff, 6, HAL_MAX_DELAY);
SET_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE);
SET_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE);
}
else if(page==4)
{
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE); //Disabling the RXNE Interrupt
CLEAR_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE); // Disabling the Idle Line Interrupt
huart2.RxState= HAL_UART_STATE_READY;
HAL_UART_Transmit(&huart2,txBuff,10,HAL_MAX_DELAY);
HAL_UART_Receive(&huart2, page4RxBuff, 6, HAL_MAX_DELAY);
SET_BIT(huart2.Instance->CR1,USART_CR1_RXNEIE);
SET_BIT(huart2.Instance->CR1,USART_CR1_IDLEIE);
}
HAL_UART_Receive_IT(&huart2, (uint8_t*)globalRxBuff, 100);
}

 

 

This code above sometimes work and sometimes it does not trigger the callback function.

At the time when it is not working, it is stuck in HAL_UART_IRQHandler function & when I go through the code step by step in debug mode, at some point it gets back into the while loop & starts working again.

Has anyone else experienced such issue?

Is there any problem in the code above?

Desperately in need of help!

Thanks in Advance..

This topic has been closed for replies.

1 reply

Pavel A.
March 21, 2024

This is a Very Frequently Asked Question.

Short answer: HAL_UARTEx_ReceiveToIdle_IT is not convenient to use as-is in most real life cases. Either use other functions, especially circular DMA - HAL_UARTEx_ReceiveToIdle_DMA  - or roll your own.