Need help spinning up an old project
Hi all,
I've been tasked with making some changes to an existing STM32 project. Unfortunately my predecessor was not keen on documentation, so I don't have much guidance on how the project was built in the past.
I have pulled the project from our SVN server and imported it into STM32CubeIDE (v1.15.0) without errors. When I attempt to build the project I get the following:
12:59:49 **** Build of configuration Default for project APM ****
make all
Cannot run program "make": Launching failed
Error: Program "make" not found in PATH
PATH=[C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE//plugins/com.st.stm32cube.ide.jre.win64_3.1.0.202310310920/jre/bin/server;C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE//plugins/com.st.stm32cube.ide.jre.win64_3.1.0.202310310920/jre/bin;C:\Program Files (x86)\STMicroelectronics\stlink_server;C:\ST\STM32CubeCLT_1.15.0;C:\ST\STM32CubeCLT_1.15.0\CMake\bin;C:\ST\STM32CubeCLT_1.15.0\Ninja\bin;C:\ST\STM32CubeCLT_1.15.0\GNU-tools-for-STM32\bin;C:\ST\STM32CubeCLT_1.15.0\STLink-gdb-server\bin;C:\ST\STM32CubeCLT_1.15.0\STM32CubeProgrammer\bin;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH\;C:\Program Files\dotnet\;C:\Program Files\Microsoft SQL Server\130\Tools\Binn\;C:\Program Files\Microsoft SQL Server\Client SDK\ODBC\170\Tools\Binn\;C:\Program Files\PuTTY\;C:\Program Files\TortoiseSVN\bin;C:\Program Files\TortoiseGit\bin;C:\Program Files\Git\cmd;C:\Users\tcarney\AppData\Local\Microsoft\WindowsApps;;C:\Dev\MOT-APM\APM;]
12:59:49 Build Failed. 1 errors, 0 warnings. (took 103ms)
However I am not sure where this PATH variable is held. The project properties shows nothing at all under 'Build Variables' and under 'Envoronment' only shows CWD and PWD.
I have tried changing the build command from default to 'C:\projects\compilers\GnuWin32\bin\make.exe' where I know that the GNU make executable exists, and then I get the following:
13:07:04 **** Build of configuration Default for project APM ****
"C:\\projects\\compilers\\GnuWin32\\bin\\make.exe" all
The system cannot find the path specified.
make: *** [gccversion] Error 1
"C:/projects/compilers/GnuWin32/bin/make.exe all" terminated with exit code 2. Build might be incomplete.
13:07:04 Build Failed. 1 errors, 0 warnings. (took 228ms)
Could anyone offer any suggestion regarding next steps that I might try to get this project to build?
Thanks