Skip to main content
Associate III
May 15, 2024
Solved

myStm login does not work

I cannot login in the STM32CubeIDE V1.15.1, it keeps falling, I have a plain private internet connection without any additional firewall than the one there is on my computer. I do not use vpn.
Everything else Works fine on the internet

i have also tried to disable my firewall, still no luck, Have also tried hotspot on my phone, no difference
I have tried all three network settings under the preferences.

I can login in the browser, but I cannot download the software for reinstall, everytime it keeps prompting me for login into stm again, even that I already is logged in.

I have tried to restart my computer several time.

On my computer at my workspace it works at it should.

This topic has been closed for replies.
STOne-32
STOne-32Best answer
ST Technical Moderator
June 17, 2024

Dear @Kvang ,

Original issue solved by 17th May 2024  The CubeMX/CubeIDE login issue is resolved - STMicroelectronics Community.

Cheers,

STOne-32.

10 replies

Graduate II
May 15, 2024

Need to login to update the HAL libraries...Need to login to update the HAL libraries...Any minute now...Any minute now...And... fail. Again.And... fail. Again.

Billy OWEN
ST Employee
May 15, 2024

Hi @Kvang 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

Graduate II
May 16, 2024

With respect, there are more of us than just Kvang with this problem. This is impeding our ability to do any work here. Thanks.

Visitor II
May 16, 2024

I'm also having the same issue.

rclendan
Graduate II
May 16, 2024

I am also completely out of commision due to this error. 

Graduate II
May 16, 2024

same issue for 2 days now, for un unnecesssary lock. why having to log Cube ??? If it cannot log, let it run.

rclendan
Graduate II
May 16, 2024

I'm still down... I can log in through the web site, but the CubeIDE (1.15.1) will not log in. It hangs and says the network is down. I have no proxy, VPN, or firewall blocks. I am working on a new design and can't generate code from the ioc file if not logged in. I would strongly recommend making login optional for critical tasks and just keep retrying in the background.

NOTE: I had another system that was logging in on its own at startup just fine. I stupily logged out to see if the problem was machine specific and now that system won't log in either.

UPDATE: Can confirm the error occurs on both Linux and Windows versions. It seems to be on the Server side.

Explorer II
May 16, 2024

Same issue here.

Huge bummer having just picked up an STM board for the first time...

Graduate II
May 16, 2024

workaround: install CubeIDE 1.12.1

It has no login functionnality and use latest packages.

if Cube MX is not conveniant, you can open your IOC file in a text writer and change this line

MxCube.Version=6.8.1

to your version.

STOne-32
STOne-32Best answer
ST Technical Moderator
June 17, 2024

Dear @Kvang ,

Original issue solved by 17th May 2024  The CubeMX/CubeIDE login issue is resolved - STMicroelectronics Community.

Cheers,

STOne-32.