Skip to main content
SidPrice
Associate III
March 15, 2023
Solved

My imported project build fails, how to fix it?

I have imported an STM32 project, created and debugged in the past using STM32CubeIDE. When I try to build this project in VSCode I see:

Executing task: Build 

build task started....

"C:\Program Files\CMake\bin\cmake.EXE" --build "D:/DataRoot/Projects/IO Technologies/IHP Controller/build/debug/build"

The parameter is incorrect

CMake Error: Generator: execution of make failed. Make command was: && 

build finished with error(s).

No changes were made to the imported project.

Please advise how to proceed.

Sid

This topic has been closed for replies.
robotdad
robotdadBest answer
Visitor II
March 23, 2023

This looks like it might be an issue with our integration of vcpkg with the Embedded Tools extension. Can you report this here so we can dig into it?

https://github.com/microsoft/vscode-embedded-tools/issues

11 replies

CsBe
Explorer II
March 28, 2023

Tryed with other network.. still the same.

> Bundled version of vcpkg: "2023-03-14-105f7f7e8a5ea10dfac9874ff9d1a6bacba5f454".

> Running vcpkg with arguments ["activate","--project","c:\\UserData\\modules\\firmware\\module-1","--json","C:\\Users\\user\\AppData\\Local\\Temp\\44c05403cd0283ca8dd043378a3e08aa"].

warning: vcpkg-artifacts is experimental and may change at any time.

node:internal/modules/cjs/loader:1078

 throw err;

 ^

Error: Cannot find module 'chalk'

Require stack:

- C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\cli\format.js

- C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\cli\command-line.js

- C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\main.js

  at Module._resolveFilename (node:internal/modules/cjs/loader:1075:15)

  at Module._load (node:internal/modules/cjs/loader:920:27)

  at Module.require (node:internal/modules/cjs/loader:1141:19)

  at require (node:internal/modules/cjs/helpers:110:18)

  at Object.<anonymous> (C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\cli\format.js:6:17)

  at Module._compile (node:internal/modules/cjs/loader:1254:14)

  at Module._extensions..js (node:internal/modules/cjs/loader:1308:10)

  at Module.load (node:internal/modules/cjs/loader:1117:32)

  at Module._load (node:internal/modules/cjs/loader:958:12)

  at Module.require (node:internal/modules/cjs/loader:1141:19) {

 code: 'MODULE_NOT_FOUND',

 requireStack: [

  'C:\\Users\\user\\AppData\\Local\\vcpkg\\artifacts-2023-03-14\\node_modules\\vcpkg-ce\\ce\\dist\\cli\\format.js',

  'C:\\Users\\user\\AppData\\Local\\vcpkg\\artifacts-2023-03-14\\node_modules\\vcpkg-ce\\ce\\dist\\cli\\command-line.js',

  'C:\\Users\\user\\AppData\\Local\\vcpkg\\artifacts-2023-03-14\\node_modules\\vcpkg-ce\\ce\\dist\\main.js'

 ]

}

Node.js v18.15.0

> Failed with exit code "1".

> Failed to activate environment at "c:\path\vcpkg-configuration.json".