My Cube is broke
- 3 replies
- 1076 views
I've tried reinstalling, uninstalling, running as root, dozens of other things... just getting these issues regardless of anything I try. As far as operation... it will start, but would bind up at 19% on a build. After reinstalling, it now takes forever figuring out the compiler languages, then, will build if I use the internal build, but not any external options. Haven't tried to upload a program, but would like to get it running normal first :\ I thought it was maybe a java update, as the log has lots of java issues, but cube brings its own java version. one thing I noticed in the logs is double slashes in the file paths. "//"... I imagine this would be an issue, but not sure why its happening. Help, please???
kali linux,,, has been working perfectly for a month now. :( Was on 1.15 when this happened. Reinstalled with 1.16. no changes. Clean pretty much freezes. takes minutes to perform each rm command to remove files, if they even complete. Seems like a permissions issue... idk logs attached.