Skip to main content
hansd56
Senior
October 21, 2019
Question

Multi core debugging

Could anybody help me how to do multi core debugging with STM32CubeIDE 1.1.0?

This topic has been closed for replies.

9 replies

Markus GIRDLAND
ST Employee
October 22, 2019

I'm working on a document to cover this topic in a bit more detail but it's not done yet. What are you having trouble with?

hansd56
hansd56Author
Senior
October 22, 2019
Hi Markus,
It would be great if you could give me a hint on how to set up the debugger. I used CubeMX to create a test project for STM32H745I-Disco. CubeIDE is very different from how System Workbench handled it.
Regards,
Hans
hansd56
hansd56Author
Senior
October 22, 2019

Thanks for your reply. I just can't download the two images. I can one by one. But then the other fails.

Markus GIRDLAND
ST Employee
October 23, 2019

How did you set up the debug configuration? In the "Startup" tab of the two sub-projects you need to make sure to click "Add..." to set up which one(s) you wish to load to the target.

hansd56
hansd56Author
Senior
October 23, 2019

I have tried this too in various configurations. I just needs some documentation to be useful. Did True Studio have a similar setup. Is the old documentation available?

Markus GIRDLAND
ST Employee
October 23, 2019

No, we didn't have it in TrueSTUDIO. All the "multi-core" device support was added just now in 1.1.0 (H7/L5/MP1) and they made a specific new feature for flashing (the Startup tab). The documentation is being made right now but MP1 and L5 has gotten prioritized and will most likely be release first.

But the basics is this, I will only mention a setting if it differs from the default.

CM7 - Debug configuration:

Debugger

Reset behaviour: Connect under reset

Tick Halt all cores

Tick Enable shared ST-LINK

Startup Tab

Add the other project

Untick Load Symbols

CM4 - Debug configuration:

Debugger

Add like +10 or something to the GDBserver (for example 61244)

Reset behaviour: None

Tick Enable shared ST-LINK

Startup Tab

Edit the CM4 project

Untick Download

Then you start to debug the CM7 and after that you launch a second debug session (without terminating CM7) with the CM4.

hansd56
hansd56Author
Senior
October 24, 2019
Thanks for your reply. It works some sort off. CM4 runs off after loading. How can you ever start both cores at the same time? They are supposed to go through a start up sequence. Cube only permits option 'Both CPU's start at once'. I can only say many nice products but nothing really finished.