Missing PWR peripheral registers in stm32g051 svd file
I've checked in svd version 1.4 : the PWR resisters are missing, just like the exti registers in this post : Solved: No GPIO registers in System Viewer drop down menu ... - STMicroelectronics Community
There are also unusual characters in some descriptions. Look at :
<name>ADRDY</name>
<description>ADC ready
This bit is set by hardware after the ADC has been enabled (ADENÂ =Â 1) and when the ADC reaches a state where it is ready to accept conversion requests.
It is cleared by software writing 1 to it.</description>
Regards,
PMZ