Skip to main content
Peter Allnutt
Associate III
May 6, 2021 1:17 PM UTC
Solved

Missing LPTIMx_OR registers when debugging L452RETx

When I try and debug my program using CubeIDE 1.6.1 there are no LPTIMx_OR registers shown in the SFR LPTIMx register blocks. Am I doing something wrong or is this broken in the debugging environment?

Using SMT32Cube MCU Package L4 1.17.0.

TIA Pete

This topic has been closed for replies.
Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
May 7, 2021 9:45 AM UTC

Hello Pete!

STM32CubeIDE only reads an .svd file to display these registers. I have submitted a ticket to the responsible team for further analysis and possible correction.

If this is urgent then you can manually add it in the .svd file by default located at:

C:\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.productdb.debug_1.6.0.202102151443\resources\cmsis\STMicroelectronics_CMSIS_SVD\STM32L4P5.svd

Thanks for bringing it to our attention!

2 replies

Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
May 7, 2021 9:45 AM UTC

Hello Pete!

STM32CubeIDE only reads an .svd file to display these registers. I have submitted a ticket to the responsible team for further analysis and possible correction.

If this is urgent then you can manually add it in the .svd file by default located at:

C:\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.productdb.debug_1.6.0.202102151443\resources\cmsis\STMicroelectronics_CMSIS_SVD\STM32L4P5.svd

Thanks for bringing it to our attention!

Peter Allnutt
Associate III
May 7, 2021 9:58 AM UTC

Thanks for getting back to me. Will do the update as you suggest.